RoutingPartLibraryNodeType Enumeration

NXOpen.Preferences.RoutingPartLibrary.NodeType is an alias for NXOpen.Preferences.RoutingPartLibraryNodeType

class NXOpen.Preferences.RoutingPartLibraryNodeType

Bases: object

Type of nodes in the part library.

Enum Members

Doesn’t have any part table information. “
“Table”, ” Part table node. Contains columns/rows that
specify parts. “
“Part”, ” Part node, contains information necessary

for loading/using a routing part. “

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.