RoutingPartFabricationNumbering Enumeration

NXOpen.Preferences.RoutingPart.FabricationNumbering is an alias for NXOpen.Preferences.RoutingPartFabricationNumbering

class NXOpen.Preferences.RoutingPartFabricationNumbering

Bases: object

The fabrication numbering methods available for the Routing bill of material.

Enum Members

Enum Member Enum Member Description
Sequence
Sequential numbering of fabrications in the parts list.
Original
Use the fabrication number in the parts list.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.