RoutingPartPreferredPortMethod Enumeration¶
NXOpen.Preferences.RoutingPart.PreferredPortMethod is an alias for NXOpen.Preferences.RoutingPartPreferredPortMethod
-
class
NXOpen.Preferences.
RoutingPartPreferredPortMethod
¶ Bases:
object
Available methods for determining which port is the preferredport during calculation of placement solutions.
Enum Members
port, and match it’s value to a desired value. “
“Name”, ” Compare the ports name with a desired value. “-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-