CollarPlateBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
CollarPlateBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.CollarPlate
builder.This builder is used to create and edit collar plate feature. The collar plate feature can be created from a profile cutout feature.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateCollarPlateBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AngularTolerance |
|
DistanceTolerance |
|
InstallDirection |
|
ManufacturingStock |
|
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProfileCutout |
|
SectionData |
|
ShipNames |
|
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
WeldCharacteristics |
|
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
UpdateCollarPlateSizeInformation |
|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngularTolerance¶
-
CollarPlateBuilder.
AngularTolerance
¶ Returns or sets the angular tolerance (degrees)
The angular tolerance is used for:
- collar plate placement orign and orientation evaluation
- collar plate geometry construction
-------------------------------------
Getter Method
Signature
AngularTolerance()
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularTolerance(angularTolerance)
Parameters: angularTolerance (float) – New in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
DistanceTolerance¶
-
CollarPlateBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance (part units)
The distance tolerance is used for:
- collar plate placement orign and orientation evaluation
- collar plate geometry construction
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
InstallDirection¶
-
CollarPlateBuilder.
InstallDirection
¶ Returns or sets the install direction.
The install direction defines which side (molding face side or opposite molding face side) the collar plate is attached to the plate.
-------------------------------------
Getter Method
Signature
InstallDirection()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InstallDirection(installDirection)
Parameters: installDirection ( NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
) –New in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
ManufacturingStock¶
-
CollarPlateBuilder.
ManufacturingStock
¶ Returns the manufacturing stock.
The manufacturing stock defines data that is to be applied to the collar plate.
-------------------------------------
Getter Method
Signature
ManufacturingStock()
Returns: Return type: NXOpen.Features.ShipDesign.ManufacturingStockBuilder
New in version NX11.0.0.
License requirements: None.
ProfileCutout¶
-
CollarPlateBuilder.
ProfileCutout
¶ Returns the profile cutout.
-------------------------------------
Getter Method
Signature
ProfileCutout()
Returns: Return type: NXOpen.ScCollector
New in version NX11.0.0.
License requirements: None.
SectionData¶
-
CollarPlateBuilder.
SectionData
¶ Returns the section data.
The section data defines the shape of the collar plate and expressions to control the size of the collar plate.
-------------------------------------
Getter Method
Signature
SectionData()
Returns: Return type: NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
New in version NX11.0.0.
License requirements: None.
ShipNames¶
-
CollarPlateBuilder.
ShipNames
¶ Returns the ship name.
The ship name is used to assign name to the collar plate.
It is only used in Ship Structure Basic Design Application.
-------------------------------------
Getter Method
Signature
ShipNames()
Returns: Ship Names Builder Return type: NXOpen.Features.ShipDesign.ShipNamesBuilder
New in version NX11.0.0.
License requirements: None.
WeldCharacteristics¶
-
CollarPlateBuilder.
WeldCharacteristics
¶ Returns the weld characteristics.
The weld characteristics defines data that is to be applied to the collar plate weld edges.
-------------------------------------
Getter Method
Signature
WeldCharacteristics()
Returns: Return type: NXOpen.Weld.CharacteristicsBuilder
New in version NX11.0.0.
License requirements: None.
Method Detail¶
UpdateCollarPlateSizeInformation¶
-
CollarPlateBuilder.
UpdateCollarPlateSizeInformation
¶ Updates collar plate size from the context information.
The collar plate size depends on the profile cutout size.
Signature
UpdateCollarPlateSizeInformation()
New in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
Validate¶
-
CollarPlateBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.