ManufacturingStockBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ManufacturingStockBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.ShipDesign.ManufacturingStockBuilder
builder.It is used to manage the data contained in the ship manufacturing stock.
This class is sub-object of another builder, and cannot be directly instantiated.
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
DataSource | Returns or sets the data source from which the intial data is read. |
DataSourceType | Returns or sets the data source from which the initial data is read. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditDataItem | Edits data item. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
InitializeDataFromDataSource | Resets the builder data from the data source. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ManufacturingStockBuilderCheckBoxStatus Enumeration | the check box status. |
ManufacturingStockBuilderLockedStatus Enumeration | the NX attribute locked status. |
ManufacturingStockBuilderObjectType Enumeration | the object to which the manufacturing attributes will be written. |
ManufacturingStockBuilderStockDataSourceType Enumeration | the data source from which the intial manufacturing data will be read. |
Property Detail¶
DataSource¶
-
ManufacturingStockBuilder.
DataSource
¶ Returns or sets the data source from which the intial data is read.
-------------------------------------
Getter Method
Signature
DataSource()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DataSource(dataSource)
Parameters: dataSource (str) – New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
DataSourceType¶
-
ManufacturingStockBuilder.
DataSourceType
¶ Returns or sets the data source from which the initial data is read.
-------------------------------------
Getter Method
Signature
DataSourceType()
Returns: Return type: NXOpen.Features.ShipDesign.ManufacturingStockBuilderStockDataSourceType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DataSourceType(dataSourceType)
Parameters: dataSourceType ( NXOpen.Features.ShipDesign.ManufacturingStockBuilderStockDataSourceType
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
Method Detail¶
EditDataItem¶
-
ManufacturingStockBuilder.
EditDataItem
¶ Edits data item.
Signature
EditDataItem(name, eCheckBoxStatus, valueNew)
Parameters: - name (str) – Item name
- eCheckBoxStatus (
NXOpen.Features.ShipDesign.ManufacturingStockBuilderCheckBoxStatus
) – New check box status. - valueNew (str) – New Value
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
InitializeDataFromDataSource¶
-
ManufacturingStockBuilder.
InitializeDataFromDataSource
¶ Resets the builder data from the data source.
Signature
InitializeDataFromDataSource(eDataSourceType, dataSource)
Parameters: - eDataSourceType (
NXOpen.Features.ShipDesign.ManufacturingStockBuilderStockDataSourceType
) – Data source type. - dataSource (str) – Data source.
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
- eDataSourceType (
Validate¶
-
ManufacturingStockBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.