BracketBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
BracketBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.Bracket
builder.This builder is used to create and edit bracket feature.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateBracketBuilder()
Default values.
Property Value AlignmentAngle.Value 0 AlignmentType DatumPlaneAlignment BracketOffset.Value 0 (millimeters part), 0 (inches part) LimitType NoLimit New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AlignmentAngle |
|
AlignmentPlane |
|
AlignmentType |
|
AngularTolerance |
|
AttachmentDirection |
|
AttachmentFace |
|
AttachmentStiffener |
|
BracketOffset |
|
DistanceTolerance |
|
EndAttachment |
|
LimitType |
|
ManufacturingStock |
|
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PickPointOnAttachment |
|
PickPointOnReinforcement |
|
ReinforcementDirection |
|
ReinforcementFace |
|
SectionData |
|
ShipNames |
|
StartAttachment |
|
StartAttachmentLimit |
|
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
ThicknessDirection |
|
WeldCharacteristics |
|
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BracketBuilderAlignmentTypes Enumeration |
|
BracketBuilderLimitTypes Enumeration |
|
Property Detail¶
AlignmentAngle¶
-
BracketBuilder.
AlignmentAngle
¶ Returns the alignment angle along attachment entity.
The bracket edge on reinforcement face side is rotated by this angle along the bracket edge on the attachment side.
The unit is in degree.
-------------------------------------
Getter Method
Signature
AlignmentAngle()
Returns: Alignment angle Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
AlignmentPlane¶
-
BracketBuilder.
AlignmentPlane
¶ Returns the alignment plane.
The bracket molding face is aligned to the alignment plane if no offset is set in
NXOpen.Features.ShipDesign.BracketBuilder.BracketOffset`()
It is only used when
NXOpen.Features.ShipDesign.BracketBuilder.AlignmentType`()
is set toFeatures.ShipDesign.BracketBuilderAlignmentTypes.DatumPlaneAlignment
.-------------------------------------
Getter Method
Signature
AlignmentPlane()
Returns: Alignment plane Return type: NXOpen.SelectDisplayableObject
New in version NX11.0.0.
License requirements: None.
AlignmentType¶
-
BracketBuilder.
AlignmentType
¶ Returns or sets the bracket alignment type.
If you set the alignment type to
Features.ShipDesign.BracketBuilderAlignmentTypes.DatumPlaneAlignment
, then please also set values for below properties:NXOpen.Features.ShipDesign.BracketBuilder.ReinforcementFace`()
NXOpen.Features.ShipDesign.BracketBuilder.AttachmentFace`()
NXOpen.Features.ShipDesign.BracketBuilder.AlignmentPlane`()
If you set the alignment type to
Features.ShipDesign.BracketBuilderAlignmentTypes.AutoAlignment
, then please also set values for below properties:NXOpen.Features.ShipDesign.BracketBuilder.ReinforcementFace`()
NXOpen.Features.ShipDesign.BracketBuilder.AttachmentStiffener`()
-------------------------------------
Getter Method
Signature
AlignmentType()
Returns: Alignment type Return type: NXOpen.Features.ShipDesign.BracketBuilderAlignmentTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignmentType(alignmentType)
Parameters: alignmentType ( NXOpen.Features.ShipDesign.BracketBuilderAlignmentTypes
) – Alignment typeNew in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
AngularTolerance¶
-
BracketBuilder.
AngularTolerance
¶ Returns or sets the angular tolerance (degrees)
The angular tolerance is used for:
- bracket placement orign and orientation evaluation
- bracket geometry construction
-------------------------------------
Getter Method
Signature
AngularTolerance()
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularTolerance(angularTolerance)
Parameters: angularTolerance (float) – New in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
AttachmentDirection¶
-
BracketBuilder.
AttachmentDirection
¶ Returns or sets the install direction on attachment face.
The attachment direction defines which side the bracket is attached to the attachment face. You can either place the bracket on the attachment face normal side or the opposite side. The install directions are ship orientations based on the attachment face normal. For example: If the attachment face normal is in ‘For’ direction, then you should set the install direction to either ‘For’ or ‘Aft’.
It is only used in Ship Structure Basic Design Application.
It is only used when
NXOpen.Features.ShipDesign.BracketBuilder.AlignmentType`()
is set toFeatures.ShipDesign.BracketBuilderAlignmentTypes.DatumPlaneAlignment
.-------------------------------------
Getter Method
Signature
AttachmentDirection()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AttachmentDirection(attachmentDirection)
Parameters: attachmentDirection ( NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
) –New in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
AttachmentFace¶
-
BracketBuilder.
AttachmentFace
¶ Returns the attachment face.
The attachment face defines the faces which the bracket is attached to. You can attach the bracket to more than one faces.
The attachment face is only used when
NXOpen.Features.ShipDesign.BracketBuilder.AlignmentType`()
is set toFeatures.ShipDesign.BracketBuilderAlignmentTypes.DatumPlaneAlignment
.-------------------------------------
Getter Method
Signature
AttachmentFace()
Returns: Return type: NXOpen.ScCollector
New in version NX11.0.0.
License requirements: None.
AttachmentStiffener¶
-
BracketBuilder.
AttachmentStiffener
¶ Returns the attachment stiffener.
The bracket is attached to the stiffener body top face and aligned to the stiffener molding face if no offset is set in
NXOpen.Features.ShipDesign.BracketBuilder.BracketOffset`()
It is only used when
NXOpen.Features.ShipDesign.BracketBuilder.AlignmentType`()
is set toFeatures.ShipDesign.BracketBuilderAlignmentTypes.AutoAlignment
.-------------------------------------
Getter Method
Signature
AttachmentStiffener()
Returns: Attachment stiffener Return type: NXOpen.SelectDisplayableObjectList
New in version NX11.0.0.
License requirements: None.
BracketOffset¶
-
BracketBuilder.
BracketOffset
¶ Returns the offset to the alignment plane or attachment stiffener molding face.
If offset is zero, the bracket molding face is aligned to the alignment plane or attachment stiffener molding face.
-------------------------------------
Getter Method
Signature
BracketOffset()
Returns: Bracket offset Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
DistanceTolerance¶
-
BracketBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance (part units)
The distance tolerance is used for:
- bracket placement orign and orientation evaluation
- bracket geometry construction
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
EndAttachment¶
-
BracketBuilder.
EndAttachment
¶ Returns the end attachment.
This defines the limit object on the end side.
It is used when
NXOpen.Features.ShipDesign.BracketBuilder.LimitType`()
is set toNXOpen.Features.ShipDesign.BracketBuilderLimitTypes.TwoLimit
orNXOpen.Features.ShipDesign.BracketBuilderLimitTypes.ThreeLimit
.-------------------------------------
Getter Method
Signature
EndAttachment()
Returns: End attachment Return type: NXOpen.ScCollector
New in version NX11.0.0.
License requirements: None.
LimitType¶
-
BracketBuilder.
LimitType
¶ Returns or sets the limit type.
If you set the limit type to
Features.ShipDesign.BracketBuilderLimitTypes.NoLimit
, you don’t need to set any limit object.If you set the limit type to
Features.ShipDesign.BracketBuilderLimitTypes.OneLimit
, then please also set value forNXOpen.Features.ShipDesign.BracketBuilder.StartAttachment`()
.If you set the alignment type to
Features.ShipDesign.BracketBuilderLimitTypes.TwoLimit
, then please also set values for below properties:NXOpen.Features.ShipDesign.BracketBuilder.StartAttachment`()
NXOpen.Features.ShipDesign.BracketBuilder.EndAttachment`()
If you set the alignment type to
NXOpen.Features.ShipDesign.BracketBuilderLimitTypes.ThreeLimit
, then please also set values for below properties:NXOpen.Features.ShipDesign.BracketBuilder.StartAttachment`()
NXOpen.Features.ShipDesign.BracketBuilder.EndAttachment`()
NXOpen.Features.ShipDesign.BracketBuilder.StartAttachmentLimit`()
-------------------------------------
Getter Method
Signature
LimitType()
Returns: Limit type Return type: NXOpen.Features.ShipDesign.BracketBuilderLimitTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitType(limitType)
Parameters: limitType ( NXOpen.Features.ShipDesign.BracketBuilderLimitTypes
) – Limit typeNew in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
ManufacturingStock¶
-
BracketBuilder.
ManufacturingStock
¶ Returns the manufacturing stock.
The manufacturing stock defines data that is to be applied to the bracket.
-------------------------------------
Getter Method
Signature
ManufacturingStock()
Returns: Manufacturing stock Return type: NXOpen.Features.ShipDesign.ManufacturingStockBuilder
New in version NX11.0.0.
License requirements: None.
PickPointOnAttachment¶
-
BracketBuilder.
PickPointOnAttachment
¶ Returns or sets the pick point on attachment face.
When the attachment face is curved (such as a cylindrical face), the bracket can be placed at multiple locations, then the pick point is used. The position which is closest to the pick point is used.
It is optional. If there are multiple candidate locations and this is not set, a random location is chosen.
It is only used when
NXOpen.Features.ShipDesign.BracketBuilder.AlignmentType`()
is set toFeatures.ShipDesign.BracketBuilderAlignmentTypes.DatumPlaneAlignment
.-------------------------------------
Getter Method
Signature
PickPointOnAttachment()
Returns: Return type: NXOpen.Point3d
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PickPointOnAttachment(pickPoint)
Parameters: pickPoint ( NXOpen.Point3d
) –New in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
PickPointOnReinforcement¶
-
BracketBuilder.
PickPointOnReinforcement
¶ Returns or sets the pick point on reinforcement face.
When the reinforcement face is curved (such as a cylindrical face), the bracket can be placed at multiple locations, then the pick point is used. The location which is closest to the pick point is used.
It is optional. If there are multiple candidate locations and this is not set, a random location is chosen.
-------------------------------------
Getter Method
Signature
PickPointOnReinforcement()
Returns: Pick Point type Return type: NXOpen.Point3d
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PickPointOnReinforcement(pickPoint)
Parameters: pickPoint ( NXOpen.Point3d
) – Pick Point typeNew in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
ReinforcementDirection¶
-
BracketBuilder.
ReinforcementDirection
¶ Returns or sets the install direction on reinforcement face.
The reinforcement direction defines which side the bracket is placed on the reinforcement face. You can either place the bracket on the reinforcement face normal side or the opposite side. The install directions are ship orientations based on the reinforcement face normal. For example: If the reinforcement face normal is in ‘For’ direction, then you should set the install direction to either ‘For’ or ‘Aft’.
It is only used in Ship Structure Basic Design Application.
-------------------------------------
Getter Method
Signature
ReinforcementDirection()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReinforcementDirection(reinforcementDirection)
Parameters: reinforcementDirection ( NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
) –New in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
ReinforcementFace¶
-
BracketBuilder.
ReinforcementFace
¶ Returns the reinforcement face.
The reinforcement face defines the objects which need to be reinforced. More than one faces can be reinforced by the bracket.
-------------------------------------
Getter Method
Signature
ReinforcementFace()
Returns: Reinforcement face Return type: NXOpen.ScCollector
New in version NX11.0.0.
License requirements: None.
SectionData¶
-
BracketBuilder.
SectionData
¶ Returns the section data.
The section data defines the shape of the bracket and expressions to control the size of the bracket.
-------------------------------------
Getter Method
Signature
SectionData()
Returns: Section data Return type: NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
New in version NX11.0.0.
License requirements: None.
ShipNames¶
-
BracketBuilder.
ShipNames
¶ Returns the ship name.
The ship name is used to assign name to the bracket.
It is only used in Ship Structure Basic Design Application.
-------------------------------------
Getter Method
Signature
ShipNames()
Returns: Ship names Return type: NXOpen.Features.ShipDesign.ShipNamesBuilder
New in version NX11.0.0.
License requirements: None.
StartAttachment¶
-
BracketBuilder.
StartAttachment
¶ Returns the start attachment.
This defines the limit object on the start side.
It is used when
NXOpen.Features.ShipDesign.BracketBuilder.LimitType`()
is set toNXOpen.Features.ShipDesign.BracketBuilderLimitTypes.OneLimit
orNXOpen.Features.ShipDesign.BracketBuilderLimitTypes.TwoLimit
orNXOpen.Features.ShipDesign.BracketBuilderLimitTypes.ThreeLimit
.-------------------------------------
Getter Method
Signature
StartAttachment()
Returns: Start attachment Return type: NXOpen.ScCollector
New in version NX11.0.0.
License requirements: None.
StartAttachmentLimit¶
-
BracketBuilder.
StartAttachmentLimit
¶ Returns the start attachment limit.
This defines the limit object on the start attachment entity.
It is used when
NXOpen.Features.ShipDesign.BracketBuilder.LimitType`()
is set toNXOpen.Features.ShipDesign.BracketBuilderLimitTypes.ThreeLimit
.-------------------------------------
Getter Method
Signature
StartAttachmentLimit()
Returns: Start attachment limit Return type: NXOpen.ScCollector
New in version NX11.0.0.
License requirements: None.
ThicknessDirection¶
-
BracketBuilder.
ThicknessDirection
¶ Returns or sets the thickness direction.
-------------------------------------
Getter Method
Signature
ThicknessDirection()
Returns: Thickness direction Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessDirection(thicknessDirection)
Parameters: thicknessDirection ( NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
) – Thickness directionNew in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
WeldCharacteristics¶
-
BracketBuilder.
WeldCharacteristics
¶ Returns the weld characteristics.
The weld characteristics defines data that is to be applied to the bracket weld edges.
-------------------------------------
Getter Method
Signature
WeldCharacteristics()
Returns: Weld characteristics Return type: NXOpen.Weld.CharacteristicsBuilder
New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
BracketBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.