NSidedSurfaceBuilder Class¶
-
class
NXOpen.Features.
NSidedSurfaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.NSidedSurface
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateNSidedSurfaceBuilder()
Default values.
Property Value CenterControlFlat.Value 100 CenterControlTiltX.Value 50 CenterControlTiltY.Value 50 CenterControlTrimFlat.Value 50 CenterControlX.Value 50 CenterControlY.Value 50 CenterControlZ.Value 50 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CenterControlFlat | Returns the center control flat |
CenterControlTiltX | Returns the center control tilt x direction |
CenterControlTiltY | Returns the center control tilt y direction |
CenterControlTrimFlat | Returns the center control flat for trimming |
CenterControlX | Returns the center control x direction |
CenterControlY | Returns the center control y direction |
CenterControlZ | Returns the center control z direction |
ConstraintFaces | Returns the constraint faces |
Continuity | Returns the continuity |
CurvatureTolerance | Returns or sets the curvature tolerance |
FlowDirection | Returns or sets the flow direction |
InteriorCurveList | Returns the list of interior curves |
MergeFaces | Returns or sets the merge-faces option |
OrientationVector | Returns or sets the orientation vector. |
OuterLoop | Returns the outer loop |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PositionTolerance | Returns or sets the position tolerance |
RectanglePointFirst | Returns or sets the first rectangle point. |
RectanglePointSecond | Returns or sets the second rectangle point. |
RectanglePointThird | Returns or sets the third rectangle point. |
SpineCurve | Returns the spine curve. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TangentTolerance | Returns or sets the tangent tolerance |
TrimToBoundary | Returns or sets the trim-to-boundary option |
Type | Returns or sets the surface type |
UVOrientation | Returns or sets the UV orientation |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
NSidedSurfaceBuilderCenterControlAxisType Enumeration | the center control types |
NSidedSurfaceBuilderCenterControlType Enumeration | the center control type options |
NSidedSurfaceBuilderFlowDirectionType Enumeration | the flow direction options |
NSidedSurfaceBuilderSurfaceType Enumeration | the surface type options |
NSidedSurfaceBuilderUVOrientationType Enumeration | the UV orientation options |
Property Detail¶
CenterControlFlat¶
-
NSidedSurfaceBuilder.
CenterControlFlat
¶ Returns the center control flat
-------------------------------------
Getter Method
Signature
CenterControlFlat()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
CenterControlTiltX¶
-
NSidedSurfaceBuilder.
CenterControlTiltX
¶ Returns the center control tilt x direction
-------------------------------------
Getter Method
Signature
CenterControlTiltX()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
CenterControlTiltY¶
-
NSidedSurfaceBuilder.
CenterControlTiltY
¶ Returns the center control tilt y direction
-------------------------------------
Getter Method
Signature
CenterControlTiltY()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
CenterControlTrimFlat¶
-
NSidedSurfaceBuilder.
CenterControlTrimFlat
¶ Returns the center control flat for trimming
-------------------------------------
Getter Method
Signature
CenterControlTrimFlat()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
CenterControlX¶
-
NSidedSurfaceBuilder.
CenterControlX
¶ Returns the center control x direction
-------------------------------------
Getter Method
Signature
CenterControlX()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
CenterControlY¶
-
NSidedSurfaceBuilder.
CenterControlY
¶ Returns the center control y direction
-------------------------------------
Getter Method
Signature
CenterControlY()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
CenterControlZ¶
-
NSidedSurfaceBuilder.
CenterControlZ
¶ Returns the center control z direction
-------------------------------------
Getter Method
Signature
CenterControlZ()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
ConstraintFaces¶
-
NSidedSurfaceBuilder.
ConstraintFaces
¶ Returns the constraint faces
-------------------------------------
Getter Method
Signature
ConstraintFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
Continuity¶
-
NSidedSurfaceBuilder.
Continuity
¶ Returns the continuity
-------------------------------------
Getter Method
Signature
Continuity()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
CurvatureTolerance¶
-
NSidedSurfaceBuilder.
CurvatureTolerance
¶ Returns or sets the curvature tolerance
-------------------------------------
Getter Method
Signature
CurvatureTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
CurvatureTolerance(curvatureTolerance)
Parameters: curvatureTolerance (float) – New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
FlowDirection¶
-
NSidedSurfaceBuilder.
FlowDirection
¶ Returns or sets the flow direction
-------------------------------------
Getter Method
Signature
FlowDirection()
Returns: Return type: NXOpen.Features.NSidedSurfaceBuilderFlowDirectionType
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
FlowDirection(button)
Parameters: button ( NXOpen.Features.NSidedSurfaceBuilderFlowDirectionType
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
InteriorCurveList¶
-
NSidedSurfaceBuilder.
InteriorCurveList
¶ Returns the list of interior curves
-------------------------------------
Getter Method
Signature
InteriorCurveList()
Returns: Return type: NXOpen.SectionList
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
MergeFaces¶
-
NSidedSurfaceBuilder.
MergeFaces
¶ Returns or sets the merge-faces option
-------------------------------------
Getter Method
Signature
MergeFaces()
Returns: Return type: bool New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
MergeFaces(mergeFaces)
Parameters: mergeFaces (bool) – New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
OrientationVector¶
-
NSidedSurfaceBuilder.
OrientationVector
¶ Returns or sets the orientation vector.
This is used only if UVOrientation is UVOrientationType.Vector
-------------------------------------
Getter Method
Signature
OrientationVector()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
OrientationVector(orientationVector)
Parameters: orientationVector ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”), nx_freeform_1 (“basic freeform modeling”)
OuterLoop¶
-
NSidedSurfaceBuilder.
OuterLoop
¶ Returns the outer loop
-------------------------------------
Getter Method
Signature
OuterLoop()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
PositionTolerance¶
-
NSidedSurfaceBuilder.
PositionTolerance
¶ Returns or sets the position tolerance
-------------------------------------
Getter Method
Signature
PositionTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
PositionTolerance(positionTolerance)
Parameters: positionTolerance (float) – New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
RectanglePointFirst¶
-
NSidedSurfaceBuilder.
RectanglePointFirst
¶ Returns or sets the first rectangle point.
This is used only if UVOrientation is UVOrientationType.Area
-------------------------------------
Getter Method
Signature
RectanglePointFirst()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
RectanglePointFirst(firstPoint)
Parameters: firstPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
RectanglePointSecond¶
-
NSidedSurfaceBuilder.
RectanglePointSecond
¶ Returns or sets the second rectangle point.
This is used only if UVOrientation is UVOrientationType.Area
-------------------------------------
Getter Method
Signature
RectanglePointSecond()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
RectanglePointSecond(secondPoint)
Parameters: secondPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
RectanglePointThird¶
-
NSidedSurfaceBuilder.
RectanglePointThird
¶ Returns or sets the third rectangle point.
This is used only if UVOrientation is UVOrientationType.Area
-------------------------------------
Getter Method
Signature
RectanglePointThird()
Returns: Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
RectanglePointThird(thirdPoint)
Parameters: thirdPoint ( NXOpen.Point
) –New in version NX8.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
SpineCurve¶
-
NSidedSurfaceBuilder.
SpineCurve
¶ Returns the spine curve.
This is used only if UVOrientation is UVOrientationType.Spine
-------------------------------------
Getter Method
Signature
SpineCurve()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
TangentTolerance¶
-
NSidedSurfaceBuilder.
TangentTolerance
¶ Returns or sets the tangent tolerance
-------------------------------------
Getter Method
Signature
TangentTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
TangentTolerance(tangentTolerance)
Parameters: tangentTolerance (float) – New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
TrimToBoundary¶
-
NSidedSurfaceBuilder.
TrimToBoundary
¶ Returns or sets the trim-to-boundary option
-------------------------------------
Getter Method
Signature
TrimToBoundary()
Returns: Return type: bool New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
TrimToBoundary(trimToBoundary)
Parameters: trimToBoundary (bool) – New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
Type¶
-
NSidedSurfaceBuilder.
Type
¶ Returns or sets the surface type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.NSidedSurfaceBuilderSurfaceType
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
Type(surfaceType)
Parameters: surfaceType ( NXOpen.Features.NSidedSurfaceBuilderSurfaceType
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
UVOrientation¶
-
NSidedSurfaceBuilder.
UVOrientation
¶ Returns or sets the UV orientation
-------------------------------------
Getter Method
Signature
UVOrientation()
Returns: Return type: NXOpen.Features.NSidedSurfaceBuilderUVOrientationType
New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
UVOrientation(button)
Parameters: button ( NXOpen.Features.NSidedSurfaceBuilderUVOrientationType
) –New in version NX6.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
Method Detail¶
Validate¶
-
NSidedSurfaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.