NSidedSurfaceBuilderCenterControlAxisType Enumeration

NXOpen.Features.NSidedSurfaceBuilder.CenterControlAxisType is an alias for NXOpen.Features.NSidedSurfaceBuilderCenterControlAxisType

class NXOpen.Features.NSidedSurfaceBuilderCenterControlAxisType

Bases: object

the center control types

Enum Members

Enum Member Enum Member Description
X
x axis
Y
y axis
Z
z axis
Flat
center flat
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.