NSidedSurfaceBuilderFlowDirectionType Enumeration

NXOpen.Features.NSidedSurfaceBuilder.FlowDirectionType is an alias for NXOpen.Features.NSidedSurfaceBuilderFlowDirectionType

class NXOpen.Features.NSidedSurfaceBuilderFlowDirectionType

Bases: object

the flow direction options

Enum Members

Enum Member Enum Member Description
NotSpecified
not specified
Perpendicular
perpendicular
IsoUVLine
uv line
AdjacentEdges
adjacent edges
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.