NSidedSurfaceBuilderUVOrientationType Enumeration

NXOpen.Features.NSidedSurfaceBuilder.UVOrientationType is an alias for NXOpen.Features.NSidedSurfaceBuilderUVOrientationType

class NXOpen.Features.NSidedSurfaceBuilderUVOrientationType

Bases: object

the UV orientation options

Enum Members

Enum Member Enum Member Description
Spine
spine orientation
Vector
vector orientation
Area
area orientation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.