AnnotateViewsBuilder Class |
This class is used to annotate views based on the knowledge fusion rules. |
AttributeItemBuilder Class |
Represents a NXOpen.Drafting.AttributeItemBuilder . |
AttributeItemBuilderList Class |
Represents a list of objects. |
AutomationManager Class |
Represents a NXOpen.Drafting.AutomationManager . |
AutomationPreferencesBuilder Class |
the builder for Drafting Automation Preferences |
AutomationRuleBuilder Class |
Represents a NXOpen.Drafting.AutomationRuleBuilder |
BaseEditSettingsBuilder Class |
Represents a NXOpen.Drafting.BaseEditSettingsBuilder . |
CutCopyPasteBuilder Class |
Represents a paste in Drafting. |
CutCopyPasteLeaderBuilder Class |
Represents a Drafting Paste, especially when reassociating a leader on paste. |
DistributeAnnotationsBuilder Class |
This class is used to distribute annotations associated to a view. |
DraftingApplicationManager Class |
Represents an object that manages drafting objects and member views. |
DrawingAutomationWizard Class |
Represents callback data for the drawing automation wizard. |
DrawingCreationWizardBuilder Class |
Represents a NXOpen.Drafting.DrawingCreationWizardBuilder . |
MoveToDrawingViewBuilder Class |
This builder allows the user to extract contents from a sheet and transfer them to a new Drawing view, also provide some other options for view creation |
PreferencesBuilder Class |
Represents a NXOpen.Drafting.PreferencesBuilder builder |
PrimaryContentItemBuilder Class |
Represents a NXOpen.Drafting.PrimaryContentItemBuilder . |
PrimaryContentItemBuilderList Class |
Represents a list of objects. |
RulesBuilder Class |
This class is used to specify knowledge fusion rules in a drawing template. |
SettingsManager Class |
Represents an object that manages drafting settings. |
SmashDrawingViewBuilder Class |
This builder allows the user to break a Drawing View into its parts and delete the Drawing View |
SpecifyRuleBuilder Class |
This class is used to specify knowledge fusion rule for a note object in a drawing template. |