AnnotateViewsBuilder Class¶
-
class
NXOpen.Drafting.
AnnotateViewsBuilder
¶ Bases:
NXOpen.Builder
This class is used to annotate views based on the knowledge fusion rules.
To create a new instance of this class, use
NXOpen.Drafting.AutomationManager.CreateAnnotateViewsBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ExistingAutomaticAnnotationOption | Returns or sets the existing automatic annotation option |
Tag | Returns the Tag for this object. |
Views | Returns the views to annotate |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AnnotateViewsBuilderExistingAutomaticAnnotation Enumeration | Option to delete or preserve existing automatic annotations when annotation views command is run. |
Property Detail¶
ExistingAutomaticAnnotationOption¶
-
AnnotateViewsBuilder.
ExistingAutomaticAnnotationOption
¶ Returns or sets the existing automatic annotation option
-------------------------------------
Getter Method
Signature
ExistingAutomaticAnnotationOption()
Returns: Return type: NXOpen.Drafting.AnnotateViewsBuilderExistingAutomaticAnnotation
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExistingAutomaticAnnotationOption(existingAutomaticAnnotationOption)
Parameters: existingAutomaticAnnotationOption ( NXOpen.Drafting.AnnotateViewsBuilderExistingAutomaticAnnotation
) –New in version NX8.0.0.
License requirements: nx_drawing_auto (“NX Drawing Automation”)
Views¶
-
AnnotateViewsBuilder.
Views
¶ Returns the views to annotate
-------------------------------------
Getter Method
Signature
Views()
Returns: Return type: NXOpen.Drawings.SelectDraftingViewList
New in version NX8.0.0.
License requirements: nx_drawing_auto (“NX Drawing Automation”)
Method Detail¶
Validate¶
-
AnnotateViewsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.