PrimaryContentItemBuilderList Class

class NXOpen.Drafting.PrimaryContentItemBuilderList

Bases: NXOpen.TaggedObject

Represents a list of objects.

To create a new instance of this class, use NXOpen.Part.CreateObjectList()

New in version NX4.0.0.

Properties

Property Description
Length Returns the length of the list
Tag Returns the Tag for this object.

Methods

Method Description
Append Appends a set of objects to the list
Clear Clears the entire list
ClearIndex Deletes the item at the index specified.
Erase Erases the object from the list, but does not delete the object.
FindIndex Finds the index where the input object appears.
FindItem Returns the object at the input index.
GetContents Gets the contents of the entire list @return The list contents
Insert Inserts an object at the specified location
MoveToBottom Move object at the specified location to the bottom of the list.
MoveToTop Move object at the specified location to the top of the list.
SetContents Sets the contents of the entire list.
Swap Exchanges the position of two objects inside the list.

Property Detail

Length

PrimaryContentItemBuilderList.Length

Returns the length of the list

-------------------------------------

Getter Method

Signature Length()

Returns:
Return type:int

New in version NX5.0.0.

License requirements: None.

Method Detail

Append

PrimaryContentItemBuilderList.Append

Overloaded method Append

  • Append(objects)
  • Append(object)

-------------------------------------

Appends a set of objects to the list

Signature Append(objects)

Parameters:objects (list of NXOpen.Drafting.PrimaryContentItemBuilder) – items to append

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Appends an object to the list

Signature Append(object)

Parameters:object (NXOpen.Drafting.PrimaryContentItemBuilder) – item to append

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Clear

PrimaryContentItemBuilderList.Clear

Overloaded method Clear

  • Clear()
  • Clear(deleteOption)

-------------------------------------

Clears the entire list

Signature Clear()

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Clears the entire list

Signature Clear(deleteOption)

Parameters:deleteOption (NXOpen.ObjectListDeleteOption) – whether to delete the objects when removing them

New in version NX5.0.0.

License requirements: None.

-------------------------------------

ClearIndex

PrimaryContentItemBuilderList.ClearIndex

Deletes the item at the index specified.

The size of the list does * not change, but the item at this index is set to NULL.

Signature ClearIndex(deleteIdx)

Parameters:deleteIdx (int) – index of item to be deleted

New in version NX4.0.0.

License requirements: None.

Erase

PrimaryContentItemBuilderList.Erase

Overloaded method Erase

  • Erase(index)
  • Erase(index, deleteOption)
  • Erase(obj)
  • Erase(obj, deleteOption)

-------------------------------------

Erases the object from the list, but does not delete the object. The list is shifted so that there isn’t a null where the object used to be.

Signature Erase(index)

Parameters:index (int) – index of item to be removed from the list

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Erases the object at the given position from the list. The list is shifted so that there isn’t a null where the object used to be.

Signature Erase(index, deleteOption)

Parameters:

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Erases the object from the list, but does not delete the object. The list is shifted so that there isn’t a null where the object used to exist.

Signature Erase(obj)

Parameters:obj (NXOpen.Drafting.PrimaryContentItemBuilder) – object to be removed from the list

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Erases the object from the list. The list is shifted so that there isn’t a null where the object used to exist.

Signature Erase(obj, deleteOption)

Parameters:

New in version NX5.0.0.

License requirements: None.

-------------------------------------

FindIndex

PrimaryContentItemBuilderList.FindIndex

Finds the index where the input object appears.

If it does not appear, * -1 is returned.

Signature FindIndex(obj)

Parameters:obj (NXOpen.Drafting.PrimaryContentItemBuilder) – Object to find index for
Returns:index of input object, -1 if not on list
Return type:int

New in version NX4.0.0.

License requirements: None.

FindItem

PrimaryContentItemBuilderList.FindItem

Returns the object at the input index.

May be NULL.

Signature FindItem(index)

Parameters:index (int) – index of object to return
Returns:object found at input index
Return type:NXOpen.Drafting.PrimaryContentItemBuilder

New in version NX4.0.0.

License requirements: None.

GetContents

PrimaryContentItemBuilderList.GetContents

Gets the contents of the entire list

Signature GetContents()

Returns:The list contents
Return type:list of NXOpen.Drafting.PrimaryContentItemBuilder

New in version NX5.0.0.

License requirements: None.

Insert

PrimaryContentItemBuilderList.Insert

Inserts an object at the specified location

Signature Insert(location, object)

Parameters:

New in version NX5.0.0.

License requirements: None.

MoveToBottom

PrimaryContentItemBuilderList.MoveToBottom

Move object at the specified location to the bottom of the list.

Signature MoveToBottom(index)

Parameters:index (int) – location of the item

New in version NX10.0.0.

License requirements: None.

MoveToTop

PrimaryContentItemBuilderList.MoveToTop

Move object at the specified location to the top of the list.

Signature MoveToTop(index)

Parameters:index (int) – location of the item

New in version NX10.0.0.

License requirements: None.

SetContents

PrimaryContentItemBuilderList.SetContents

Sets the contents of the entire list.

This overwrites the previous contents of this list, but does not delete any objects that were originally on the list.

Signature SetContents(objects)

Parameters:objects (list of NXOpen.Drafting.PrimaryContentItemBuilder) – The list contents

New in version NX5.0.0.

License requirements: None.

Swap

PrimaryContentItemBuilderList.Swap

Overloaded method Swap

  • Swap(index1, index2)
  • Swap(object1, object2)

-------------------------------------

Exchanges the position of two objects inside the list. The first object is placed where the second used to be, and second object where the first used to be.

Signature Swap(index1, index2)

Parameters:
  • index1 (int) – location of the first item
  • index2 (int) – location of the second item

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Exchanges the position of two objects inside the list. The first object is placed where the second used to be, and second object where the first used to be.

Signature Swap(object1, object2)

Parameters:

New in version NX5.0.0.

License requirements: None.

-------------------------------------