PrimaryContentItemBuilder Class

class NXOpen.Drafting.PrimaryContentItemBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Drafting.PrimaryContentItemBuilder.

This class is used to specify information pertaining to the primary content of a Drawing Booklet. Each instance represents a single drawing in a booklet.

To create a new instance of this class, use NXOpen.Drafting.AutomationManager.CreatePrimaryContentItemBuilder()

New in version NX8.0.0.

Properties

Property Description
Content Returns the content.
GeometryTemplate Returns or sets the geometry template.
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

Content

PrimaryContentItemBuilder.Content

Returns the content.

-------------------------------------

Getter Method

Signature Content()

Returns:
Return type:NXOpen.Assemblies.SelectComponentList

New in version NX8.0.0.

License requirements: None.

GeometryTemplate

PrimaryContentItemBuilder.GeometryTemplate

Returns or sets the geometry template.

-------------------------------------

Getter Method

Signature GeometryTemplate()

Returns:
Return type:str

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature GeometryTemplate(geometryTemplate)

Parameters:geometryTemplate (str) –

New in version NX8.0.0.

License requirements: nx_drawing_auto (“NX Drawing Automation”)

Method Detail

Validate

PrimaryContentItemBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.