CutCopyPasteBuilderTypePaste Enumeration

NXOpen.Drafting.CutCopyPasteBuilder.TypePaste is an alias for NXOpen.Drafting.CutCopyPasteBuilderTypePaste

class NXOpen.Drafting.CutCopyPasteBuilderTypePaste

Bases: object

Specifies the paste type.

Enum Members

Enum Member Enum Member Description
Transform
Transform type
Tracking
Tracking type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.