Preferences Class¶
-
class
NXOpen.CAM.
Preferences
¶ Bases:
NXOpen.Builder
Represents a cam preferences Builder
To create a new instance of this class, use
NXOpen.CAM.CAMSession.CreateCamPreferences()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AlwaysUpdateDialogs | Returns or sets the auto update dialog |
AutomaticallySetMachingData | Returns or sets the auto maching data |
AuxiliaryFloorColor | Returns or sets the auxiliary floor |
AuxiliaryFloorColorSelection | Returns or sets the auxiliary floor selection. |
BladeBlendColor | Returns or sets the blade blend color |
BladeColor | Returns or sets the blade color |
BlankColor | Returns or sets the blank color |
BlankSelection | Returns or sets the blank selection. |
CheckColor | Returns or sets the check color |
CheckSelection | Returns or sets the check selection. |
ClearanceColor | Returns or sets the clearance color |
ClsfDecimals | Returns or sets the clsf_decimals |
ClsfForceLoadTurret | Returns or sets the force load turret |
ConfigurationFile | Returns or sets the configuration file |
CsysInformationListing | Returns or sets the base info |
CsysOrientWcsToMcs | Returns or sets the orient wcs to mcs |
CutAreaColor | Returns or sets the cut area color |
CutAreaSelection | Returns or sets the cut area selection. |
DisplaySelectedObjects | Returns or sets the display selected objects |
DisplayTurningIpw | Returns or sets the display turning ipw |
DriveColor | Returns or sets the drive color |
EnableLevelBasedIpw | Returns or sets the enable level based ipw |
ForceRegenerate | Returns or sets the force regenerate |
GeneratePaths | Returns or sets the generate tool paths |
GenerationFullRegeneration | Returns or sets the full regeneration |
GenerationPauseAfterEachPath | Returns or sets the pause after each path |
GenerationRefreshBeforeEachPath | Returns or sets the refresh before each path |
GenerationSmartRegeneration | Returns or sets the smart regeneration |
GenerationUpdateInstances | Returns or sets the update all instances |
HubColor | Returns or sets the hub color |
IncludeInstances | Returns or sets the include instances |
IpwNeedleCountCoarse | Returns or sets the coarse ipw needle count |
IpwNeedleCountFine | Returns or sets the fine ipw needle count |
IpwNeedleCountMedium | Returns or sets the medium ipw needle count |
IpwNeedleDistanceCoarse | Returns or sets the coarse ipw needle distance |
IpwNeedleDistanceFine | Returns or sets the fine ipw needle distance |
IpwNeedleDistanceMedium | Returns or sets the medium ipw needle distance |
IpwPartsFolder | Returns or sets the ipw parts folder |
IpwToleranceMode | Returns or sets the ipw tolerance mode |
IpwUseDirectoryOfOriginalPart | Returns or sets the use directory original part |
LinkMcsRcs | Returns or sets the link mcs rcs |
OptimizedCutLevelColor | Returns or sets the optimized cut level |
PartColor | Returns or sets the part color |
PartSelection | Returns or sets the part selection. |
RelocateParameters | Returns or sets the relocate parameters |
ReplayRefreshBeforeEachPath | Returns or sets the refresh before each path replay |
RunProcessAssistant | Returns or sets the process assistant |
SaveIpwModel | Returns or sets the ipw model |
SaveLevelBasedIpw | Returns or sets the level based ipw |
ScrollAreaSize | Returns or sets the scrollable items |
ShowPictures | Returns or sets the show pictures |
ShroudColor | Returns or sets the shroud color |
SplitterColor | Returns or sets the splitter color |
SuspectBoundingBoxColor | Returns or sets the suspect bounding box color |
Tag | Returns the Tag for this object. |
TemplateFile | Returns or sets the template file |
TopOffLevelColor | Returns or sets the top off level |
TrimColor | Returns or sets the trim color |
UncutRegionColor | Returns or sets the uncut region color |
UnlinkInstances | Returns or sets the unlink instances |
Visualize2dTool1Color | Returns or sets the tool color1 |
Visualize2dTool2Color | Returns or sets the tool color2 |
Visualize2dTool3Color | Returns or sets the tool color3 |
Visualize2dTool4Color | Returns or sets the tool color4 |
Visualize2dTool5Color | Returns or sets the tool color5 |
VisualizeAnimationAccuracy | Returns or sets the animation accuracy |
VisualizeAutoBlockColor | Returns or sets the auto block color |
VisualizeBackgroundColor | Returns or sets the background color |
VisualizeChordalTolerance | Returns or sets the chordal tolerance |
VisualizeCollisionsColor | Returns or sets the collisions color |
VisualizeDynamicToolAxis | Returns or sets the dynamic tool axis |
VisualizeExcessMaterialColor | Returns or sets the excess material color |
VisualizeGougesColor | Returns or sets the gouges color |
VisualizeIpwColor | Returns or sets the ipw color |
VisualizeIpwDmrColor1 | Returns or sets the ipw dmr color1 |
VisualizeIpwDmrColor10 | Returns or sets the ipw dmr color10 |
VisualizeIpwDmrColor2 | Returns or sets the ipw dmr color2 |
VisualizeIpwDmrColor3 | Returns or sets the ipw dmr color3 |
VisualizeIpwDmrColor4 | Returns or sets the ipw dmr color4 |
VisualizeIpwDmrColor5 | Returns or sets the ipw dmr color5 |
VisualizeIpwDmrColor6 | Returns or sets the ipw dmr color6 |
VisualizeIpwDmrColor7 | Returns or sets the ipw dmr color7 |
VisualizeIpwDmrColor8 | Returns or sets the ipw dmr color8 |
VisualizeIpwDmrColor9 | Returns or sets the ipw dmr color9 |
VisualizeIpwDmrColoringMode | Returns or sets the ipw dmr coloring mode |
VisualizeIpwTranslucency | Returns or sets the ipw translucency |
VisualizeSafeToolColor | Returns or sets the safe tool color |
VisualizeTemporaryContainmentCurveColor | Returns or sets the temporary containment curve color |
VisualizeToolAxisTiltTolerance | Returns or sets the tilt tolerance |
VisualizeToolDisplayColor | Returns or sets the tool display color |
VisualizeToolEditAndDisplay | Returns or sets the tool edit and display |
VisualizeToolHolderColor | Returns or sets the tool holder color |
VisualizeToolInsertOrFluteColor | Returns or sets the turning tool insert |
VisualizeToolShankColor | Returns or sets the tool shank color |
VisualizeToolTranslucency | Returns or sets the tool translucency |
WallColor | Returns or sets the wall color |
WallSelection | Returns or sets the wall selection. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDefaultConfigurationFile | Get the default configuration file @return |
GetDefaultIpwFolder | Get the ipw default folder @return |
GetDefaultTemplateFile | Get the default template file @return |
GetObject | Returns the object currently being edited by this builder. |
GetSelection | The geometry selection type method @return |
SetSelection | The geometry selection type method |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PreferencesAnimationAccuracyTypes Enumeration | the animation accuracy types |
PreferencesAuxiliaryFloorColorSelectionTypes Enumeration | the auxiliary floor selection types. |
PreferencesBlankSelectionTypes Enumeration | the blank selection types. |
PreferencesCheckSelectionTypes Enumeration | the check selection types. |
PreferencesCsysInformationListingTypes Enumeration | the information listing types |
PreferencesCutAreaSelectionTypes Enumeration | the cut area selection types. |
PreferencesGeometryTypes Enumeration | the geometry types |
PreferencesIpwDmrColoringTypes Enumeration | the IPW material removal coloring types |
PreferencesIpwToleranceModeTypes Enumeration | the IPW tolerance modes |
PreferencesPartSelectionTypes Enumeration | the part selection types. |
PreferencesSelectionTypes Enumeration | the selection types |
PreferencesWallSelectionTypes Enumeration | the wall selection types. |
Property Detail¶
AlwaysUpdateDialogs¶
-
Preferences.
AlwaysUpdateDialogs
¶ Returns or sets the auto update dialog
-------------------------------------
Getter Method
Signature
AlwaysUpdateDialogs()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlwaysUpdateDialogs(alwaysUpdateDialogs)
Parameters: alwaysUpdateDialogs (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
AutomaticallySetMachingData¶
-
Preferences.
AutomaticallySetMachingData
¶ Returns or sets the auto maching data
-------------------------------------
Getter Method
Signature
AutomaticallySetMachingData()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutomaticallySetMachingData(autoMachingData)
Parameters: autoMachingData (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
AuxiliaryFloorColor¶
-
Preferences.
AuxiliaryFloorColor
¶ Returns or sets the auxiliary floor
-------------------------------------
Getter Method
Signature
AuxiliaryFloorColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AuxiliaryFloorColor(auxiliaryFloor)
Parameters: auxiliaryFloor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
AuxiliaryFloorColorSelection¶
-
Preferences.
AuxiliaryFloorColorSelection
¶ Returns or sets the auxiliary floor selection.
-------------------------------------
Getter Method
Signature
AuxiliaryFloorColorSelection()
Returns: Return type: NXOpen.CAM.PreferencesAuxiliaryFloorColorSelectionTypes
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
AuxiliaryFloorColorSelection(auxiliaryFloorSelection)
Parameters: auxiliaryFloorSelection ( NXOpen.CAM.PreferencesAuxiliaryFloorColorSelectionTypes
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: cam_base (“CAM BASE”)
BladeBlendColor¶
-
Preferences.
BladeBlendColor
¶ Returns or sets the blade blend color
-------------------------------------
Getter Method
Signature
BladeBlendColor()
Returns: Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BladeBlendColor(bladeBlend)
Parameters: bladeBlend (Id) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
BladeColor¶
-
Preferences.
BladeColor
¶ Returns or sets the blade color
-------------------------------------
Getter Method
Signature
BladeColor()
Returns: Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BladeColor(blade)
Parameters: blade (Id) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
BlankColor¶
-
Preferences.
BlankColor
¶ Returns or sets the blank color
-------------------------------------
Getter Method
Signature
BlankColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankColor(blankColor)
Parameters: blankColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
BlankSelection¶
-
Preferences.
BlankSelection
¶ Returns or sets the blank selection.
-------------------------------------
Getter Method
Signature
BlankSelection()
Returns: Return type: NXOpen.CAM.PreferencesBlankSelectionTypes
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
BlankSelection(blankSelection)
Parameters: blankSelection ( NXOpen.CAM.PreferencesBlankSelectionTypes
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: cam_base (“CAM BASE”)
CheckColor¶
-
Preferences.
CheckColor
¶ Returns or sets the check color
-------------------------------------
Getter Method
Signature
CheckColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CheckColor(checkColor)
Parameters: checkColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CheckSelection¶
-
Preferences.
CheckSelection
¶ Returns or sets the check selection.
-------------------------------------
Getter Method
Signature
CheckSelection()
Returns: Return type: NXOpen.CAM.PreferencesCheckSelectionTypes
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
CheckSelection(checkSelection)
Parameters: checkSelection ( NXOpen.CAM.PreferencesCheckSelectionTypes
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: cam_base (“CAM BASE”)
ClearanceColor¶
-
Preferences.
ClearanceColor
¶ Returns or sets the clearance color
-------------------------------------
Getter Method
Signature
ClearanceColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClearanceColor(clearanceColor)
Parameters: clearanceColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ClsfDecimals¶
-
Preferences.
ClsfDecimals
¶ Returns or sets the clsf_decimals
-------------------------------------
Getter Method
Signature
ClsfDecimals()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClsfDecimals(decimals)
Parameters: decimals (int) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ClsfForceLoadTurret¶
-
Preferences.
ClsfForceLoadTurret
¶ Returns or sets the force load turret
-------------------------------------
Getter Method
Signature
ClsfForceLoadTurret()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClsfForceLoadTurret(forceLoadTurret)
Parameters: forceLoadTurret (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ConfigurationFile¶
-
Preferences.
ConfigurationFile
¶ Returns or sets the configuration file
-------------------------------------
Getter Method
Signature
ConfigurationFile()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConfigurationFile(fileName)
Parameters: fileName (str) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CsysInformationListing¶
-
Preferences.
CsysInformationListing
¶ Returns or sets the base info
-------------------------------------
Getter Method
Signature
CsysInformationListing()
Returns: Return type: NXOpen.CAM.PreferencesCsysInformationListingTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysInformationListing(baseInfo)
Parameters: baseInfo ( NXOpen.CAM.PreferencesCsysInformationListingTypes
) –New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CsysOrientWcsToMcs¶
-
Preferences.
CsysOrientWcsToMcs
¶ Returns or sets the orient wcs to mcs
-------------------------------------
Getter Method
Signature
CsysOrientWcsToMcs()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysOrientWcsToMcs(orientWcsToMcs)
Parameters: orientWcsToMcs (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CutAreaColor¶
-
Preferences.
CutAreaColor
¶ Returns or sets the cut area color
-------------------------------------
Getter Method
Signature
CutAreaColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutAreaColor(cutAreaColor)
Parameters: cutAreaColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CutAreaSelection¶
-
Preferences.
CutAreaSelection
¶ Returns or sets the cut area selection.
-------------------------------------
Getter Method
Signature
CutAreaSelection()
Returns: Return type: NXOpen.CAM.PreferencesCutAreaSelectionTypes
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
CutAreaSelection(cutAreaSelection)
Parameters: cutAreaSelection ( NXOpen.CAM.PreferencesCutAreaSelectionTypes
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: cam_base (“CAM BASE”)
DisplaySelectedObjects¶
-
Preferences.
DisplaySelectedObjects
¶ Returns or sets the display selected objects
-------------------------------------
Getter Method
Signature
DisplaySelectedObjects()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplaySelectedObjects(displaySelectedObjects)
Parameters: displaySelectedObjects (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
DisplayTurningIpw¶
-
Preferences.
DisplayTurningIpw
¶ Returns or sets the display turning ipw
-------------------------------------
Getter Method
Signature
DisplayTurningIpw()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayTurningIpw(displayTurningIpw)
Parameters: displayTurningIpw (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
DriveColor¶
-
Preferences.
DriveColor
¶ Returns or sets the drive color
-------------------------------------
Getter Method
Signature
DriveColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DriveColor(driveColor)
Parameters: driveColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
EnableLevelBasedIpw¶
-
Preferences.
EnableLevelBasedIpw
¶ Returns or sets the enable level based ipw
-------------------------------------
Getter Method
Signature
EnableLevelBasedIpw()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnableLevelBasedIpw(enableLevelBasedIpw)
Parameters: enableLevelBasedIpw (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ForceRegenerate¶
-
Preferences.
ForceRegenerate
¶ Returns or sets the force regenerate
-------------------------------------
Getter Method
Signature
ForceRegenerate()
Returns: Return type: bool New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
ForceRegenerate(isForceRegenerate)
Parameters: isForceRegenerate (bool) – New in version NX10.0.3.
License requirements: cam_base (“CAM BASE”)
GeneratePaths¶
-
Preferences.
GeneratePaths
¶ Returns or sets the generate tool paths
-------------------------------------
Getter Method
Signature
GeneratePaths()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GeneratePaths(generatePaths)
Parameters: generatePaths (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
GenerationFullRegeneration¶
-
Preferences.
GenerationFullRegeneration
¶ Returns or sets the full regeneration
-------------------------------------
Getter Method
Signature
GenerationFullRegeneration()
Returns: Return type: bool New in version NX9.0.3.
Deprecated since version NX10.0.3: Use
CAM.Preferences.GenerationSmartRegeneration()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
GenerationFullRegeneration(fullRegeneration)
Parameters: fullRegeneration (bool) – New in version NX9.0.3.
Deprecated since version NX10.0.3: Use
CAM.Preferences.GenerationSmartRegeneration()
instead.License requirements: cam_base (“CAM BASE”)
GenerationPauseAfterEachPath¶
-
Preferences.
GenerationPauseAfterEachPath
¶ Returns or sets the pause after each path
-------------------------------------
Getter Method
Signature
GenerationPauseAfterEachPath()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GenerationPauseAfterEachPath(pauseAfterEachPath)
Parameters: pauseAfterEachPath (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
GenerationRefreshBeforeEachPath¶
-
Preferences.
GenerationRefreshBeforeEachPath
¶ Returns or sets the refresh before each path
-------------------------------------
Getter Method
Signature
GenerationRefreshBeforeEachPath()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GenerationRefreshBeforeEachPath(refreshBeforeEachPath)
Parameters: refreshBeforeEachPath (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
GenerationSmartRegeneration¶
-
Preferences.
GenerationSmartRegeneration
¶ Returns or sets the smart regeneration
-------------------------------------
Getter Method
Signature
GenerationSmartRegeneration()
Returns: Return type: bool New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
GenerationSmartRegeneration(smartRegeneration)
Parameters: smartRegeneration (bool) – New in version NX10.0.3.
License requirements: cam_base (“CAM BASE”)
GenerationUpdateInstances¶
-
Preferences.
GenerationUpdateInstances
¶ Returns or sets the update all instances
-------------------------------------
Getter Method
Signature
GenerationUpdateInstances()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GenerationUpdateInstances(updateInstances)
Parameters: updateInstances (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
HubColor¶
-
Preferences.
HubColor
¶ Returns or sets the hub color
-------------------------------------
Getter Method
Signature
HubColor()
Returns: Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HubColor(hub)
Parameters: hub (Id) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
IncludeInstances¶
-
Preferences.
IncludeInstances
¶ Returns or sets the include instances
-------------------------------------
Getter Method
Signature
IncludeInstances()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeInstances(includeInstances)
Parameters: includeInstances (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
IpwNeedleCountCoarse¶
-
Preferences.
IpwNeedleCountCoarse
¶ Returns or sets the coarse ipw needle count
-------------------------------------
Getter Method
Signature
IpwNeedleCountCoarse()
Returns: Return type: int New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwNeedleCountCoarse(count)
Parameters: count (int) – New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwNeedleCountFine¶
-
Preferences.
IpwNeedleCountFine
¶ Returns or sets the fine ipw needle count
-------------------------------------
Getter Method
Signature
IpwNeedleCountFine()
Returns: Return type: int New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwNeedleCountFine(count)
Parameters: count (int) – New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwNeedleCountMedium¶
-
Preferences.
IpwNeedleCountMedium
¶ Returns or sets the medium ipw needle count
-------------------------------------
Getter Method
Signature
IpwNeedleCountMedium()
Returns: Return type: int New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwNeedleCountMedium(count)
Parameters: count (int) – New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwNeedleDistanceCoarse¶
-
Preferences.
IpwNeedleDistanceCoarse
¶ Returns or sets the coarse ipw needle distance
-------------------------------------
Getter Method
Signature
IpwNeedleDistanceCoarse()
Returns: Return type: float New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwNeedleDistanceCoarse(distance)
Parameters: distance (float) – New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwNeedleDistanceFine¶
-
Preferences.
IpwNeedleDistanceFine
¶ Returns or sets the fine ipw needle distance
-------------------------------------
Getter Method
Signature
IpwNeedleDistanceFine()
Returns: Return type: float New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwNeedleDistanceFine(distance)
Parameters: distance (float) – New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwNeedleDistanceMedium¶
-
Preferences.
IpwNeedleDistanceMedium
¶ Returns or sets the medium ipw needle distance
-------------------------------------
Getter Method
Signature
IpwNeedleDistanceMedium()
Returns: Return type: float New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwNeedleDistanceMedium(distance)
Parameters: distance (float) – New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwPartsFolder¶
-
Preferences.
IpwPartsFolder
¶ Returns or sets the ipw parts folder
-------------------------------------
Getter Method
Signature
IpwPartsFolder()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwPartsFolder(foldername)
Parameters: foldername (str) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
IpwToleranceMode¶
-
Preferences.
IpwToleranceMode
¶ Returns or sets the ipw tolerance mode
-------------------------------------
Getter Method
Signature
IpwToleranceMode()
Returns: Return type: NXOpen.CAM.PreferencesIpwToleranceModeTypes
New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwToleranceMode(mode)
Parameters: mode ( NXOpen.CAM.PreferencesIpwToleranceModeTypes
) –New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwUseDirectoryOfOriginalPart¶
-
Preferences.
IpwUseDirectoryOfOriginalPart
¶ Returns or sets the use directory original part
-------------------------------------
Getter Method
Signature
IpwUseDirectoryOfOriginalPart()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwUseDirectoryOfOriginalPart(useIpwDirectoryOfOriginalPart)
Parameters: useIpwDirectoryOfOriginalPart (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
LinkMcsRcs¶
-
Preferences.
LinkMcsRcs
¶ Returns or sets the link mcs rcs
-------------------------------------
Getter Method
Signature
LinkMcsRcs()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinkMcsRcs(linkMcsRcs)
Parameters: linkMcsRcs (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
OptimizedCutLevelColor¶
-
Preferences.
OptimizedCutLevelColor
¶ Returns or sets the optimized cut level
-------------------------------------
Getter Method
Signature
OptimizedCutLevelColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OptimizedCutLevelColor(optimizedCutLevel)
Parameters: optimizedCutLevel (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
PartColor¶
-
Preferences.
PartColor
¶ Returns or sets the part color
-------------------------------------
Getter Method
Signature
PartColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartColor(partColor)
Parameters: partColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
PartSelection¶
-
Preferences.
PartSelection
¶ Returns or sets the part selection.
-------------------------------------
Getter Method
Signature
PartSelection()
Returns: Return type: NXOpen.CAM.PreferencesPartSelectionTypes
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
PartSelection(partSelection)
Parameters: partSelection ( NXOpen.CAM.PreferencesPartSelectionTypes
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: cam_base (“CAM BASE”)
RelocateParameters¶
-
Preferences.
RelocateParameters
¶ Returns or sets the relocate parameters
-------------------------------------
Getter Method
Signature
RelocateParameters()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RelocateParameters(relocateParameters)
Parameters: relocateParameters (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ReplayRefreshBeforeEachPath¶
-
Preferences.
ReplayRefreshBeforeEachPath
¶ Returns or sets the refresh before each path replay
-------------------------------------
Getter Method
Signature
ReplayRefreshBeforeEachPath()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReplayRefreshBeforeEachPath(refreshBeforeEachPath)
Parameters: refreshBeforeEachPath (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
RunProcessAssistant¶
-
Preferences.
RunProcessAssistant
¶ Returns or sets the process assistant
-------------------------------------
Getter Method
Signature
RunProcessAssistant()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RunProcessAssistant(processAssistant)
Parameters: processAssistant (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
SaveIpwModel¶
-
Preferences.
SaveIpwModel
¶ Returns or sets the ipw model
-------------------------------------
Getter Method
Signature
SaveIpwModel()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveIpwModel(ipwModel)
Parameters: ipwModel (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
SaveLevelBasedIpw¶
-
Preferences.
SaveLevelBasedIpw
¶ Returns or sets the level based ipw
-------------------------------------
Getter Method
Signature
SaveLevelBasedIpw()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveLevelBasedIpw(levelBasedIpw)
Parameters: levelBasedIpw (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ScrollAreaSize¶
-
Preferences.
ScrollAreaSize
¶ Returns or sets the scrollable items
-------------------------------------
Getter Method
Signature
ScrollAreaSize()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScrollAreaSize(scrollableItems)
Parameters: scrollableItems (int) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ShowPictures¶
-
Preferences.
ShowPictures
¶ Returns or sets the show pictures
-------------------------------------
Getter Method
Signature
ShowPictures()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowPictures(showPictures)
Parameters: showPictures (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ShroudColor¶
-
Preferences.
ShroudColor
¶ Returns or sets the shroud color
-------------------------------------
Getter Method
Signature
ShroudColor()
Returns: Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShroudColor(shroud)
Parameters: shroud (Id) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
SplitterColor¶
-
Preferences.
SplitterColor
¶ Returns or sets the splitter color
-------------------------------------
Getter Method
Signature
SplitterColor()
Returns: Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SplitterColor(splitter)
Parameters: splitter (Id) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
SuspectBoundingBoxColor¶
-
Preferences.
SuspectBoundingBoxColor
¶ Returns or sets the suspect bounding box color
-------------------------------------
Getter Method
Signature
SuspectBoundingBoxColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SuspectBoundingBoxColor(suspectBoundingBoxColor)
Parameters: suspectBoundingBoxColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
TemplateFile¶
-
Preferences.
TemplateFile
¶ Returns or sets the template file
-------------------------------------
Getter Method
Signature
TemplateFile()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TemplateFile(fileName)
Parameters: fileName (str) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
TopOffLevelColor¶
-
Preferences.
TopOffLevelColor
¶ Returns or sets the top off level
-------------------------------------
Getter Method
Signature
TopOffLevelColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TopOffLevelColor(topOffLevel)
Parameters: topOffLevel (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
TrimColor¶
-
Preferences.
TrimColor
¶ Returns or sets the trim color
-------------------------------------
Getter Method
Signature
TrimColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimColor(trimColor)
Parameters: trimColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
UncutRegionColor¶
-
Preferences.
UncutRegionColor
¶ Returns or sets the uncut region color
-------------------------------------
Getter Method
Signature
UncutRegionColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UncutRegionColor(uncutRegionColor)
Parameters: uncutRegionColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
UnlinkInstances¶
-
Preferences.
UnlinkInstances
¶ Returns or sets the unlink instances
-------------------------------------
Getter Method
Signature
UnlinkInstances()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UnlinkInstances(unlinkInstances)
Parameters: unlinkInstances (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Visualize2dTool1Color¶
-
Preferences.
Visualize2dTool1Color
¶ Returns or sets the tool color1
-------------------------------------
Getter Method
Signature
Visualize2dTool1Color()
Returns: Return type: Id New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor1()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Visualize2dTool1Color(toolColor)
Parameters: toolColor (Id) – New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor1()
instead.License requirements: cam_base (“CAM BASE”)
Visualize2dTool2Color¶
-
Preferences.
Visualize2dTool2Color
¶ Returns or sets the tool color2
-------------------------------------
Getter Method
Signature
Visualize2dTool2Color()
Returns: Return type: Id New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor2()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Visualize2dTool2Color(toolColor)
Parameters: toolColor (Id) – New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor2()
instead.License requirements: cam_base (“CAM BASE”)
Visualize2dTool3Color¶
-
Preferences.
Visualize2dTool3Color
¶ Returns or sets the tool color3
-------------------------------------
Getter Method
Signature
Visualize2dTool3Color()
Returns: Return type: Id New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor3()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Visualize2dTool3Color(toolColor)
Parameters: toolColor (Id) – New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor3()
instead.License requirements: cam_base (“CAM BASE”)
Visualize2dTool4Color¶
-
Preferences.
Visualize2dTool4Color
¶ Returns or sets the tool color4
-------------------------------------
Getter Method
Signature
Visualize2dTool4Color()
Returns: Return type: Id New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor4()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Visualize2dTool4Color(toolColor)
Parameters: toolColor (Id) – New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor4()
instead.License requirements: cam_base (“CAM BASE”)
Visualize2dTool5Color¶
-
Preferences.
Visualize2dTool5Color
¶ Returns or sets the tool color5
-------------------------------------
Getter Method
Signature
Visualize2dTool5Color()
Returns: Return type: Id New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor5()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Visualize2dTool5Color(toolColor)
Parameters: toolColor (Id) – New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor5()
instead.License requirements: cam_base (“CAM BASE”)
VisualizeAnimationAccuracy¶
-
Preferences.
VisualizeAnimationAccuracy
¶ Returns or sets the animation accuracy
-------------------------------------
Getter Method
Signature
VisualizeAnimationAccuracy()
Returns: Return type: NXOpen.CAM.PreferencesAnimationAccuracyTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeAnimationAccuracy(animationAccuracy)
Parameters: animationAccuracy ( NXOpen.CAM.PreferencesAnimationAccuracyTypes
) –New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeAutoBlockColor¶
-
Preferences.
VisualizeAutoBlockColor
¶ Returns or sets the auto block color
-------------------------------------
Getter Method
Signature
VisualizeAutoBlockColor()
Returns: Return type: Id New in version NX7.5.0.
Deprecated since version NX8.5.0: Use
CAM.Preferences.BlankColor()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeAutoBlockColor(autoBlockColor)
Parameters: autoBlockColor (Id) – New in version NX7.5.0.
Deprecated since version NX8.5.0: Use
CAM.Preferences.BlankColor()
instead.License requirements: cam_base (“CAM BASE”)
VisualizeBackgroundColor¶
-
Preferences.
VisualizeBackgroundColor
¶ Returns or sets the background color
-------------------------------------
Getter Method
Signature
VisualizeBackgroundColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeBackgroundColor(backgroundColor)
Parameters: backgroundColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeChordalTolerance¶
-
Preferences.
VisualizeChordalTolerance
¶ Returns or sets the chordal tolerance
-------------------------------------
Getter Method
Signature
VisualizeChordalTolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeChordalTolerance(chordalTolerance)
Parameters: chordalTolerance (float) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeCollisionsColor¶
-
Preferences.
VisualizeCollisionsColor
¶ Returns or sets the collisions color
-------------------------------------
Getter Method
Signature
VisualizeCollisionsColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeCollisionsColor(collisionsColor)
Parameters: collisionsColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeDynamicToolAxis¶
-
Preferences.
VisualizeDynamicToolAxis
¶ Returns or sets the dynamic tool axis
-------------------------------------
Getter Method
Signature
VisualizeDynamicToolAxis()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeDynamicToolAxis(dynToolAxis)
Parameters: dynToolAxis (bool) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeExcessMaterialColor¶
-
Preferences.
VisualizeExcessMaterialColor
¶ Returns or sets the excess material color
-------------------------------------
Getter Method
Signature
VisualizeExcessMaterialColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeExcessMaterialColor(excessMaterialColor)
Parameters: excessMaterialColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeGougesColor¶
-
Preferences.
VisualizeGougesColor
¶ Returns or sets the gouges color
-------------------------------------
Getter Method
Signature
VisualizeGougesColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeGougesColor(gougesColor)
Parameters: gougesColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwColor¶
-
Preferences.
VisualizeIpwColor
¶ Returns or sets the ipw color
-------------------------------------
Getter Method
Signature
VisualizeIpwColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwColor(ipwColor)
Parameters: ipwColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor1¶
-
Preferences.
VisualizeIpwDmrColor1
¶ Returns or sets the ipw dmr color1
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor1()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor1(ipwColor)
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor10¶
-
Preferences.
VisualizeIpwDmrColor10
¶ Returns or sets the ipw dmr color10
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor10()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor10(ipwColor)
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor2¶
-
Preferences.
VisualizeIpwDmrColor2
¶ Returns or sets the ipw dmr color2
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor2()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor2(ipwColor)
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor3¶
-
Preferences.
VisualizeIpwDmrColor3
¶ Returns or sets the ipw dmr color3
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor3()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor3(ipwColor)
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor4¶
-
Preferences.
VisualizeIpwDmrColor4
¶ Returns or sets the ipw dmr color4
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor4()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor4(ipwColor)
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor5¶
-
Preferences.
VisualizeIpwDmrColor5
¶ Returns or sets the ipw dmr color5
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor5()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor5(ipwColor)
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor6¶
-
Preferences.
VisualizeIpwDmrColor6
¶ Returns or sets the ipw dmr color6
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor6()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor6(ipwColor)
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor7¶
-
Preferences.
VisualizeIpwDmrColor7
¶ Returns or sets the ipw dmr color7
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor7()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor7(ipwColor)
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor8¶
-
Preferences.
VisualizeIpwDmrColor8
¶ Returns or sets the ipw dmr color8
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor8()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor8(ipwColor)
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor9¶
-
Preferences.
VisualizeIpwDmrColor9
¶ Returns or sets the ipw dmr color9
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor9()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor9(ipwColor)
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColoringMode¶
-
Preferences.
VisualizeIpwDmrColoringMode
¶ Returns or sets the ipw dmr coloring mode
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColoringMode()
Returns: Return type: NXOpen.CAM.PreferencesIpwDmrColoringTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColoringMode(coloring)
Parameters: coloring ( NXOpen.CAM.PreferencesIpwDmrColoringTypes
) –New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwTranslucency¶
-
Preferences.
VisualizeIpwTranslucency
¶ Returns or sets the ipw translucency
-------------------------------------
Getter Method
Signature
VisualizeIpwTranslucency()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwTranslucency(ipwTranslucency)
Parameters: ipwTranslucency (int) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeSafeToolColor¶
-
Preferences.
VisualizeSafeToolColor
¶ Returns or sets the safe tool color
-------------------------------------
Getter Method
Signature
VisualizeSafeToolColor()
Returns: Return type: Id New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeSafeToolColor(safeToolColor)
Parameters: safeToolColor (Id) – New in version NX7.5.2.
License requirements: cam_base (“CAM BASE”)
VisualizeTemporaryContainmentCurveColor¶
-
Preferences.
VisualizeTemporaryContainmentCurveColor
¶ Returns or sets the temporary containment curve color
-------------------------------------
Getter Method
Signature
VisualizeTemporaryContainmentCurveColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeTemporaryContainmentCurveColor(temporaryContainmentCurveColor)
Parameters: temporaryContainmentCurveColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolAxisTiltTolerance¶
-
Preferences.
VisualizeToolAxisTiltTolerance
¶ Returns or sets the tilt tolerance
-------------------------------------
Getter Method
Signature
VisualizeToolAxisTiltTolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolAxisTiltTolerance(tiltTolerance)
Parameters: tiltTolerance (float) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolDisplayColor¶
-
Preferences.
VisualizeToolDisplayColor
¶ Returns or sets the tool display color
-------------------------------------
Getter Method
Signature
VisualizeToolDisplayColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolDisplayColor(toolDisplayColor)
Parameters: toolDisplayColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolEditAndDisplay¶
-
Preferences.
VisualizeToolEditAndDisplay
¶ Returns or sets the tool edit and display
-------------------------------------
Getter Method
Signature
VisualizeToolEditAndDisplay()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolEditAndDisplay(toolDisplayColor)
Parameters: toolDisplayColor (bool) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolHolderColor¶
-
Preferences.
VisualizeToolHolderColor
¶ Returns or sets the tool holder color
-------------------------------------
Getter Method
Signature
VisualizeToolHolderColor()
Returns: holder color Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolHolderColor(holderColor)
Parameters: holderColor (Id) – holder color New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolInsertOrFluteColor¶
-
Preferences.
VisualizeToolInsertOrFluteColor
¶ Returns or sets the turning tool insert
-------------------------------------
Getter Method
Signature
VisualizeToolInsertOrFluteColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolInsertOrFluteColor(color)
Parameters: color (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolShankColor¶
-
Preferences.
VisualizeToolShankColor
¶ Returns or sets the tool shank color
-------------------------------------
Getter Method
Signature
VisualizeToolShankColor()
Returns: shank color Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolShankColor(shankColor)
Parameters: shankColor (Id) – shank color New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolTranslucency¶
-
Preferences.
VisualizeToolTranslucency
¶ Returns or sets the tool translucency
-------------------------------------
Getter Method
Signature
VisualizeToolTranslucency()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolTranslucency(toolTranslucency)
Parameters: toolTranslucency (int) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
WallColor¶
-
Preferences.
WallColor
¶ Returns or sets the wall color
-------------------------------------
Getter Method
Signature
WallColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WallColor(wallColor)
Parameters: wallColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
WallSelection¶
-
Preferences.
WallSelection
¶ Returns or sets the wall selection.
-------------------------------------
Getter Method
Signature
WallSelection()
Returns: Return type: NXOpen.CAM.PreferencesWallSelectionTypes
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
WallSelection(wallSelection)
Parameters: wallSelection ( NXOpen.CAM.PreferencesWallSelectionTypes
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetDefaultConfigurationFile¶
-
Preferences.
GetDefaultConfigurationFile
¶ Get the default configuration file
Signature
GetDefaultConfigurationFile()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
GetDefaultIpwFolder¶
-
Preferences.
GetDefaultIpwFolder
¶ Get the ipw default folder
Signature
GetDefaultIpwFolder()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
GetDefaultTemplateFile¶
-
Preferences.
GetDefaultTemplateFile
¶ Get the default template file
Signature
GetDefaultTemplateFile()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
GetSelection¶
-
Preferences.
GetSelection
¶ The geometry selection type method
Signature
GetSelection(geomType)
Parameters: geomType ( NXOpen.CAM.PreferencesGeometryTypes
) –Returns: Return type: NXOpen.CAM.PreferencesSelectionTypes
New in version NX8.0.0.
License requirements: None.
SetSelection¶
-
Preferences.
SetSelection
¶ The geometry selection type method
Signature
SetSelection(geomType, selection)
Parameters: - geomType (
NXOpen.CAM.PreferencesGeometryTypes
) – - selection (
NXOpen.CAM.PreferencesSelectionTypes
) –
New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
- geomType (
Validate¶
-
Preferences.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.