PreferencesBlankSelectionTypes Enumeration¶
NXOpen.CAM.Preferences.BlankSelectionTypes is an alias for NXOpen.CAM.PreferencesBlankSelectionTypes
-
class
NXOpen.CAM.
PreferencesBlankSelectionTypes
¶ Bases:
object
the blank selection types.
Deprecated since version NX8.0.0: Use SelectionTypes instead.
Enum Members
Enum Member Enum Member Description Bodies BodiesFaces FacesCurves CurvesSurfaceRegion Surface RegionFacetedBodies Faceted Bodies Region-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-