PreferencesAnimationAccuracyTypes Enumeration

NXOpen.CAM.Preferences.AnimationAccuracyTypes is an alias for NXOpen.CAM.PreferencesAnimationAccuracyTypes

class NXOpen.CAM.PreferencesAnimationAccuracyTypes

Bases: object

the animation accuracy types

Enum Members

Enum Member Enum Member Description
Fine
Fine
Coarse
Coarse
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.