PreferencesCsysInformationListingTypes Enumeration

NXOpen.CAM.Preferences.CsysInformationListingTypes is an alias for NXOpen.CAM.PreferencesCsysInformationListingTypes

class NXOpen.CAM.PreferencesCsysInformationListingTypes

Bases: object

the information listing types

Enum Members

Enum Member Enum Member Description
Wcs
WCS
Mcs
MCS
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.