PreferencesGeometryTypes Enumeration

NXOpen.CAM.Preferences.GeometryTypes is an alias for NXOpen.CAM.PreferencesGeometryTypes

class NXOpen.CAM.PreferencesGeometryTypes

Bases: object

the geometry types

Enum Members

Enum Member Enum Member Description
Part
part
Blank
blank
Check
check
CutArea
cut area
AuxiliaryFloor
auxiliary floor
Walls
walls
SurfaceAreaDrive
surface area drive geometry
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.