LaserProfileMove Class¶
-
class
NXOpen.CAM.
LaserProfileMove
¶ Bases:
NXOpen.CAM.MoveBuilder
Represents a LaserProfileMove
To create a new instance of this class, use
NXOpen.CAM.MoveCollection.CreateLaserProfileMove()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CollisionCheck | Returns or sets the Collision Check |
CutDirection | Returns the Cut Direction |
FeedRate | Returns or sets the feed rate |
FeedType | Returns or sets the feed type |
FeedUnit | Returns or sets the feed unit |
HeadOrientation | Returns the Head Orientation |
InterpMethod | Returns or sets the Interpolation Method |
List | Returns the List |
MaxGapDist | Returns or sets the Max Gap Distance |
MaxTiltAngle | Returns or sets the Max Tilt Angle |
MotionType | Returns or sets the motion type |
NumberOfUserParameters | Returns the number of user parameters |
ProfileSection | Returns or sets the Profile Section |
ProtectedMove | Returns or sets the protected move status |
ShapeType | Returns or sets the Shape Type |
SubopLabel | Returns or sets the subop label |
Tag | Returns the Tag for this object. |
ToolSide | Returns or sets the Tool Side |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateControlPoint | Create a new Laser Control Point @return the control points |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetUserParameter | Returns the custom parameter with the given name. |
SetParent | Set parent |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LaserProfileMoveCollisionChecks Enumeration | the Collision Check enum |
LaserProfileMoveInterpMethods Enumeration | the Interpolation Method enum |
LaserProfileMoveShapeTypes Enumeration | the Shape Type enum |
LaserProfileMoveToolSides Enumeration | the Tool Side enum |
Property Detail¶
CollisionCheck¶
-
LaserProfileMove.
CollisionCheck
¶ Returns or sets the Collision Check
-------------------------------------
Getter Method
Signature
CollisionCheck()
Returns: the collision check Return type: NXOpen.CAM.LaserProfileMoveCollisionChecks
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CollisionCheck(type)
Parameters: type ( NXOpen.CAM.LaserProfileMoveCollisionChecks
) – the collision checkNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
CutDirection¶
-
LaserProfileMove.
CutDirection
¶ Returns the Cut Direction
-------------------------------------
Getter Method
Signature
CutDirection()
Returns: Return type: NXOpen.CAM.LaserCutDirection
New in version NX9.0.0.
License requirements: None.
HeadOrientation¶
-
LaserProfileMove.
HeadOrientation
¶ Returns the Head Orientation
-------------------------------------
Getter Method
Signature
HeadOrientation()
Returns: Return type: NXOpen.CAM.LaserHeadOrientation
New in version NX9.0.0.
License requirements: None.
InterpMethod¶
-
LaserProfileMove.
InterpMethod
¶ Returns or sets the Interpolation Method
-------------------------------------
Getter Method
Signature
InterpMethod()
Returns: the interpolation method Return type: NXOpen.CAM.LaserProfileMoveInterpMethods
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InterpMethod(type)
Parameters: type ( NXOpen.CAM.LaserProfileMoveInterpMethods
) – the interpolation methodNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
List¶
-
LaserProfileMove.
List
¶ Returns the List
-------------------------------------
Getter Method
Signature
List()
Returns: Return type: NXOpen.CAM.LaserControlPointList
New in version NX9.0.0.
License requirements: None.
MaxGapDist¶
-
LaserProfileMove.
MaxGapDist
¶ Returns or sets the Max Gap Distance
-------------------------------------
Getter Method
Signature
MaxGapDist()
Returns: the Max Gap Distance Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxGapDist(newValue)
Parameters: newValue (float) – the Max Gap Distance New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
MaxTiltAngle¶
-
LaserProfileMove.
MaxTiltAngle
¶ Returns or sets the Max Tilt Angle
-------------------------------------
Getter Method
Signature
MaxTiltAngle()
Returns: the Max Tilt Angle Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxTiltAngle(newValue)
Parameters: newValue (float) – the Max Tilt Angle New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
ProfileSection¶
-
LaserProfileMove.
ProfileSection
¶ Returns or sets the Profile Section
-------------------------------------
Getter Method
Signature
ProfileSection()
Returns: the Profile Section Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProfileSection(profileSection)
Parameters: profileSection ( NXOpen.Section
) – the Profile SectionNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
ShapeType¶
-
LaserProfileMove.
ShapeType
¶ Returns or sets the Shape Type
-------------------------------------
Getter Method
Signature
ShapeType()
Returns: the shape type Return type: NXOpen.CAM.LaserProfileMoveShapeTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShapeType(type)
Parameters: type ( NXOpen.CAM.LaserProfileMoveShapeTypes
) – the shape typeNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
ToolSide¶
-
LaserProfileMove.
ToolSide
¶ Returns or sets the Tool Side
-------------------------------------
Getter Method
Signature
ToolSide()
Returns: the tool side Return type: NXOpen.CAM.LaserProfileMoveToolSides
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolSide(type)
Parameters: type ( NXOpen.CAM.LaserProfileMoveToolSides
) – the tool sideNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
CreateControlPoint¶
-
LaserProfileMove.
CreateControlPoint
¶ Create a new Laser Control Point
Signature
CreateControlPoint(headOrientType, pointTag, csysTag, processType, toggle, udePathTag, pointType)
Parameters: - headOrientType (int) – head orient type
- pointTag (
NXOpen.Point
) – the point - csysTag (
NXOpen.CartesianCoordinateSystem
) – the csys - processType (int) – point process type
- toggle (bool) – events toggle
- udePathTag (
NXOpen.NXObject
) – the ude path - pointType (int) – point type
Returns: the control points
Return type: New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
LaserProfileMove.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.