LaserHeadOrientation Class¶
-
class
NXOpen.CAM.
LaserHeadOrientation
¶ Bases:
NXOpen.TaggedObject
Represents head orientation settings for laser sub move
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Csys | Returns or sets the Head Orientation |
OrientationType | Returns or sets the Head Orientation Type |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
LaserHeadOrientationTypes Enumeration | the Head Orientation Type enum |
Property Detail¶
Csys¶
-
LaserHeadOrientation.
Csys
¶ Returns or sets the Head Orientation
-------------------------------------
Getter Method
Signature
Csys()
Returns: the head orientation Return type: NXOpen.CartesianCoordinateSystem
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Csys(mcs)
Parameters: mcs ( NXOpen.CartesianCoordinateSystem
) – the head orientationNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
OrientationType¶
-
LaserHeadOrientation.
OrientationType
¶ Returns or sets the Head Orientation Type
-------------------------------------
Getter Method
Signature
OrientationType()
Returns: the head orientation type Return type: NXOpen.CAM.LaserHeadOrientationTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationType(type)
Parameters: type ( NXOpen.CAM.LaserHeadOrientationTypes
) – the head orientation typeNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)