LaserHeadOrientationTypes Enumeration

NXOpen.CAM.LaserHeadOrientation.Types is an alias for NXOpen.CAM.LaserHeadOrientationTypes

class NXOpen.CAM.LaserHeadOrientationTypes

Bases: object

the Head Orientation Type enum

New in version NX9.0.0.

Enum Members

Enum Member Enum Member Description
NoChange
No Change
McsZy
MCS Z/Y
Specify
Specify
Dynamic
Dynamic
NormalToPart
Normal to Part
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.