LaserProfileMoveShapeTypes Enumeration

NXOpen.CAM.LaserProfileMove.ShapeTypes is an alias for NXOpen.CAM.LaserProfileMoveShapeTypes

class NXOpen.CAM.LaserProfileMoveShapeTypes

Bases: object

the Shape Type enum

New in version NX9.0.0.

Enum Members

Enum Member Enum Member Description
ExternalTrim
External Trim
InternalTrim
Internal Trim
OpenProfile
Open Profile
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.