LaserControlPoint Class¶
-
class
NXOpen.CAM.
LaserControlPoint
¶ Bases:
NXOpen.TaggedObject
Represents a Laser Control Point builder
To create a new instance of this class, use
NXOpen.CAM.LaserProfileMove.CreateControlPoint()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Csys | Returns or sets the Local Head Orientation |
EventFlag | Returns or sets the flag whether the control event is available |
LocalHeadOrientType | Returns or sets the Local Head Orientation Type |
Point | Returns or sets the Control Point |
ProcessType | Returns or sets the Point Process Type |
Tag | Returns the Tag for this object. |
UdeSet | Returns the Machine Control Events |
Methods¶
Enumerations¶
LaserControlPointControlPointTypes Enumeration | the Control Point type |
LaserControlPointHeadOrientTypes Enumeration | the Local Head Orientation Enum |
LaserControlPointProcessTypes Enumeration | the Point Process Enumeration |
Property Detail¶
Csys¶
-
LaserControlPoint.
Csys
¶ Returns or sets the Local Head Orientation
-------------------------------------
Getter Method
Signature
Csys()
Returns: the local head orientation Return type: NXOpen.CartesianCoordinateSystem
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Csys(mcs)
Parameters: mcs ( NXOpen.CartesianCoordinateSystem
) – the local head orientationNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
EventFlag¶
-
LaserControlPoint.
EventFlag
¶ Returns or sets the flag whether the control event is available
-------------------------------------
Getter Method
Signature
EventFlag()
Returns: the logical value Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EventFlag(newValue)
Parameters: newValue (bool) – the logical value New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
LocalHeadOrientType¶
-
LaserControlPoint.
LocalHeadOrientType
¶ Returns or sets the Local Head Orientation Type
-------------------------------------
Getter Method
Signature
LocalHeadOrientType()
Returns: Return type: NXOpen.CAM.LaserControlPointHeadOrientTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocalHeadOrientType(type)
Parameters: type ( NXOpen.CAM.LaserControlPointHeadOrientTypes
) –New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
Point¶
-
LaserControlPoint.
Point
¶ Returns or sets the Control Point
-------------------------------------
Getter Method
Signature
Point()
Returns: the point Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(newValue)
Parameters: newValue ( NXOpen.Point
) – the pointNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
ProcessType¶
-
LaserControlPoint.
ProcessType
¶ Returns or sets the Point Process Type
-------------------------------------
Getter Method
Signature
ProcessType()
Returns: Return type: NXOpen.CAM.LaserControlPointProcessTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProcessType(type)
Parameters: type ( NXOpen.CAM.LaserControlPointProcessTypes
) –New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
UdeSet¶
-
LaserControlPoint.
UdeSet
¶ Returns the Machine Control Events
-------------------------------------
Getter Method
Signature
UdeSet()
Returns: Return type: NXOpen.CAM.UdeSet
New in version NX9.0.0.
License requirements: None.