LaserControlPointControlPointTypes Enumeration

NXOpen.CAM.LaserControlPoint.ControlPointTypes is an alias for NXOpen.CAM.LaserControlPointControlPointTypes

class NXOpen.CAM.LaserControlPointControlPointTypes

Bases: object

the Control Point type

New in version NX9.0.0.

Enum Members

Enum Member Enum Member Description
Sys
sys
Adj
adj
Coll
coll
Mod
mod
User
user
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.