InspectionLinkPmiBuilder Class¶
-
class
NXOpen.CAM.
InspectionLinkPmiBuilder
¶ Bases:
NXOpen.Builder
Create Link PMI Dialog Builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionLinkPmiBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
AngleA | Returns or sets the A angle |
AngleB | Returns or sets the B angle |
AngleString | Returns or sets the angle specification string |
CollisionAvoidanceEnum | Returns or sets the collision avoidance enum |
ComponentSelection | Returns the component selector |
CreatePathsEnum | Returns or sets the create paths enum |
IncludeSubComponents | Returns or sets the include sub-components option |
PathOrderEnum | Returns or sets the path order optimization type enum |
PointOrderEnum | Returns or sets the point order optimization type enum |
ProbeTipType | Returns or sets the preferred probe tip type |
ProgramLocationString | Returns or sets the program location string |
ScopeEnum | Returns or sets the scope of the Link PMI function |
Tag | Returns the Tag for this object. |
TipString | Returns or sets the tip to use for inspection string |
ToolString | Returns or sets the tool to use for inspection string |
ViewString | Returns or sets the PMI View selection string |
WorkpieceString | Returns or sets the name of the workpiece to be processed by Link PMI |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetResults | Get results from Link PMI. |
LinkToPmi | Links PMI and GDT to Inspection features and tolerances. |
OutputResults | Output results report from Link PMI. |
SafePlaneDisplayAction | Button to display selected safe plane |
SafePlaneSelectAction | Button to select safe plane |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InspectionLinkPmiBuilderCollisionAvoidanceEnumType Enumeration | Specifies whether collision avoidance will be done |
InspectionLinkPmiBuilderCreatePathsOptions Enumeration | Specifies whether paths will be created by Link PMI |
InspectionLinkPmiBuilderPathOrderTypes Enumeration | Specifies the Path Order Optimization Type |
InspectionLinkPmiBuilderPmiScopeTypes Enumeration | Specifies the scope of the link PMI command |
InspectionLinkPmiBuilderPointOrderTypes Enumeration | Specifies the Point Order Optimization Type |
Property Detail¶
AngleA¶
-
InspectionLinkPmiBuilder.
AngleA
¶ Returns or sets the A angle
-------------------------------------
Getter Method
Signature
AngleA()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleA(angleA)
Parameters: angleA (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AngleB¶
-
InspectionLinkPmiBuilder.
AngleB
¶ Returns or sets the B angle
-------------------------------------
Getter Method
Signature
AngleB()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleB(angleB)
Parameters: angleB (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AngleString¶
-
InspectionLinkPmiBuilder.
AngleString
¶ Returns or sets the angle specification string
-------------------------------------
Getter Method
Signature
AngleString()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleString(angleString)
Parameters: angleString (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ComponentSelection¶
-
InspectionLinkPmiBuilder.
ComponentSelection
¶ Returns the component selector
-------------------------------------
Getter Method
Signature
ComponentSelection()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX9.0.3.
License requirements: None.
CreatePathsEnum¶
-
InspectionLinkPmiBuilder.
CreatePathsEnum
¶ Returns or sets the create paths enum
-------------------------------------
Getter Method
Signature
CreatePathsEnum()
Returns: Return type: NXOpen.CAM.InspectionLinkPmiBuilderCreatePathsOptions
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreatePathsEnum(createPathsEnum)
Parameters: createPathsEnum ( NXOpen.CAM.InspectionLinkPmiBuilderCreatePathsOptions
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IncludeSubComponents¶
-
InspectionLinkPmiBuilder.
IncludeSubComponents
¶ Returns or sets the include sub-components option
-------------------------------------
Getter Method
Signature
IncludeSubComponents()
Returns: Return type: bool New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeSubComponents(includeSubComponents)
Parameters: includeSubComponents (bool) – New in version NX9.0.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PathOrderEnum¶
-
InspectionLinkPmiBuilder.
PathOrderEnum
¶ Returns or sets the path order optimization type enum
-------------------------------------
Getter Method
Signature
PathOrderEnum()
Returns: Return type: NXOpen.CAM.InspectionLinkPmiBuilderPathOrderTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PathOrderEnum(pathOrderEnum)
Parameters: pathOrderEnum ( NXOpen.CAM.InspectionLinkPmiBuilderPathOrderTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointOrderEnum¶
-
InspectionLinkPmiBuilder.
PointOrderEnum
¶ Returns or sets the point order optimization type enum
-------------------------------------
Getter Method
Signature
PointOrderEnum()
Returns: Return type: NXOpen.CAM.InspectionLinkPmiBuilderPointOrderTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointOrderEnum(pointOrderEnum)
Parameters: pointOrderEnum ( NXOpen.CAM.InspectionLinkPmiBuilderPointOrderTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProbeTipType¶
-
InspectionLinkPmiBuilder.
ProbeTipType
¶ Returns or sets the preferred probe tip type
-------------------------------------
Getter Method
Signature
ProbeTipType()
Returns: Return type: NXOpen.CAM.InspectionMoveBuilderProbeTipTypes
New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProbeTipType(tipType)
Parameters: tipType ( NXOpen.CAM.InspectionMoveBuilderProbeTipTypes
) –New in version NX9.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProgramLocationString¶
-
InspectionLinkPmiBuilder.
ProgramLocationString
¶ Returns or sets the program location string
-------------------------------------
Getter Method
Signature
ProgramLocationString()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProgramLocationString(programLocationString)
Parameters: programLocationString (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ScopeEnum¶
-
InspectionLinkPmiBuilder.
ScopeEnum
¶ Returns or sets the scope of the Link PMI function
-------------------------------------
Getter Method
Signature
ScopeEnum()
Returns: Return type: NXOpen.CAM.InspectionLinkPmiBuilderPmiScopeTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScopeEnum(scopeEnum)
Parameters: scopeEnum ( NXOpen.CAM.InspectionLinkPmiBuilderPmiScopeTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TipString¶
-
InspectionLinkPmiBuilder.
TipString
¶ Returns or sets the tip to use for inspection string
-------------------------------------
Getter Method
Signature
TipString()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TipString(tipString)
Parameters: tipString (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ToolString¶
-
InspectionLinkPmiBuilder.
ToolString
¶ Returns or sets the tool to use for inspection string
-------------------------------------
Getter Method
Signature
ToolString()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolString(toolString)
Parameters: toolString (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ViewString¶
-
InspectionLinkPmiBuilder.
ViewString
¶ Returns or sets the PMI View selection string
-------------------------------------
Getter Method
Signature
ViewString()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ViewString(viewString)
Parameters: viewString (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
WorkpieceString¶
-
InspectionLinkPmiBuilder.
WorkpieceString
¶ Returns or sets the name of the workpiece to be processed by Link PMI
-------------------------------------
Getter Method
Signature
WorkpieceString()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WorkpieceString(workpieceString)
Parameters: workpieceString (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
GetResults¶
-
InspectionLinkPmiBuilder.
GetResults
¶ Get results from Link PMI.
Signature
GetResults()
Returns: Results strings Return type: list of str New in version NX8.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LinkToPmi¶
-
InspectionLinkPmiBuilder.
LinkToPmi
¶ Links PMI and GDT to Inspection features and tolerances.
Signature
LinkToPmi()
New in version NX8.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OutputResults¶
-
InspectionLinkPmiBuilder.
OutputResults
¶ Output results report from Link PMI.
Signature
OutputResults(deviceType, fileName)
Parameters: - deviceType (
NXOpen.ListingWindowDeviceType
) – The type of device (file, Information window, or both) - fileName (str) – Name of the file. Used only if the device type is file or both.
New in version NX8.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
- deviceType (
SafePlaneDisplayAction¶
-
InspectionLinkPmiBuilder.
SafePlaneDisplayAction
¶ Button to display selected safe plane
Signature
SafePlaneDisplayAction()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SafePlaneSelectAction¶
-
InspectionLinkPmiBuilder.
SafePlaneSelectAction
¶ Button to select safe plane
Signature
SafePlaneSelectAction()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionLinkPmiBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.