InspectionLinkPmiBuilderCollisionAvoidanceEnumType Enumeration

NXOpen.CAM.InspectionLinkPmiBuilder.CollisionAvoidanceEnumType is an alias for NXOpen.CAM.InspectionLinkPmiBuilderCollisionAvoidanceEnumType

class NXOpen.CAM.InspectionLinkPmiBuilderCollisionAvoidanceEnumType

Bases: object

Specifies whether collision avoidance will be done

Enum Members

Enum Member Enum Member Description
Off
Collision avoidance will not be done
On
Collision avoidance will be done
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.