InspectionLinkPmiBuilderPointOrderTypes Enumeration

NXOpen.CAM.InspectionLinkPmiBuilder.PointOrderTypes is an alias for NXOpen.CAM.InspectionLinkPmiBuilderPointOrderTypes

class NXOpen.CAM.InspectionLinkPmiBuilderPointOrderTypes

Bases: object

Specifies the Point Order Optimization Type

Enum Members

Enum Member Enum Member Description
Off
No point order optimization will be done
NearestNeighbor
Point order optimization will use the nearest neighbor method
ShortestPath
Point order optimization will use the shortest path method
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.