InspectionLinkPmiBuilderPmiScopeTypes Enumeration

NXOpen.CAM.InspectionLinkPmiBuilder.PmiScopeTypes is an alias for NXOpen.CAM.InspectionLinkPmiBuilderPmiScopeTypes

class NXOpen.CAM.InspectionLinkPmiBuilderPmiScopeTypes

Bases: object

Specifies the scope of the link PMI command

Enum Members

Enum Member Enum Member Description
WorkpieceOnly
Link PMI will be performed for the workpiece only
WorkpieceandComponents
Link PMI will be performed for the workpiece and components
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.