AngularDimensionValuePrecision |
Returns or sets the angular dimension value precision |
AngularToleranceValuePrecision |
Returns or sets the angular tolerance value precision |
BaselineOffset |
Returns or sets the offset between dimension lines of baseline dimensions |
ChainOffset |
Returns or sets the offset between dimension lines of chain dimensions |
ChamferForm |
Returns or sets the chamfer dimension form |
ChamferLeaderType |
Returns or sets the chamfer dimension leader type |
ChamferSeparator |
Returns or sets the chamfer separator type |
ChamferSpaceFactor |
Returns or sets the chamfer dimension space factor |
ChamferStubType |
Returns or sets the chamfer dimension stub type |
ChamferSymbolName |
Returns or sets the chamfer dimension symbol name |
ChamferSymbolType |
Returns or sets the chamfer dimension symbol type |
DimArrowDisplay |
Returns or sets the dimension arrow display option |
DimZeroToleranceDisplayStyle |
Returns or sets the dimension zero tolerance display style |
DimensionValuePrecision |
Returns or sets the dimension value precision |
DualDimensionFractionDenominator |
Returns or sets the dual dimension fractional denominator |
DualDimensionValuePrecision |
Returns or sets the dual dimension value precision |
DualToleranceValuePrecision |
Returns or sets the dual tolerance value precision |
ExtensionLineDisplay |
Returns or sets the extension line display option. |
FitToleranceParentheses |
Returns or sets the fit tolerance parentheses option. |
FitToleranceSeparator |
Returns or sets the fit tolerance separator option. |
InspectionDimension |
Returns or sets the inspection dimension flag |
InspectionSymbolAroundAppendedText |
Returns or sets the inspection symbol around appended text option |
LimitFitAnsiHoleType |
Returns or sets the dimension limit fit ansi hole type |
LimitFitAssemblyDisplayStyle |
Returns or sets the display style of fit tolerance for assembly dimensions. |
LimitFitAssemblyNewDisplayStyle |
Returns or sets the new display style of fit tolerance for assembly dimensions. |
LimitFitDeviation |
Returns or sets the dimension limit fit deviation |
LimitFitDisplayAlignment |
Returns or sets the dimension limit fit display alignment. |
LimitFitDisplaySplitByDimline |
Returns or sets the dimension limit fit assembly display when split by dimension line. |
LimitFitDisplayStyle |
Returns or sets the dimension limit fit display style |
LimitFitGrade |
Returns or sets the dimension limit fit grade |
LimitFitShaftDeviation |
Returns or sets the shaft deviation for fit tolerance of a dimension |
LimitFitShaftGrade |
Returns or sets the shaft grade for fit tolerance of a dimension |
LineBetweenArrows |
Returns or sets the line between arrows. |
LowerToleranceDegrees |
Returns or sets the lower angular tolerance in degrees |
LowerToleranceEnglish |
Returns or sets the lower english tolerance |
LowerToleranceMetric |
Returns or sets the lower metric tolerance |
NarrowArrowType |
Returns or sets the narrow dimension arrowhead type which is used when there is no space for normal arrowheads |
NarrowDisplayType |
Returns or sets the display type for narrow dimensions |
NarrowLeaderAngle |
Returns or sets the narrow dimension leader angle |
NarrowTextOffset |
Returns or sets the narrow dimension text offset |
NarrowTextOrientation |
Returns or sets the narrow dimension text orientation |
Orientation |
Returns or sets the dimension text orientation |
OverrideDimensionText |
Returns or sets the override dimension text |
PrefixSuffixReference |
Returns or sets the flag indicating whether prefix suffix reference toggle is turned on or not |
PrimaryDimensionFractionDenominator |
Returns or sets the primary dimension fractional denominator |
ReferenceDimension |
Returns or sets the reference dimension flag |
ReferenceDimensionPrefix |
Returns or sets the prefix characters for reference dimension |
ReferenceDimensionSuffix |
Returns or sets the suffix characters for reference dimension |
ReverseArrowDirection |
Returns or sets the reverse arrow direction flag |
Tag |
Returns the Tag for this object. |
TextAngle |
Returns or sets the dimension text angle |
TextArrowPlacement |
Returns or sets the text arrow placement. |
TextCentered |
Returns or sets the dimension text centered option |
TextPosition |
Returns or sets the dimension text position representing above or after stub |
ToleranceType |
Returns or sets the dimension tolerance type |
ToleranceValuePrecision |
Returns or sets the tolerance value precision |
TrimDimLine |
Returns or sets the trim dimension line flag. |
TrueLengthText |
Returns or sets the true length dimension text |
TrueLengthTextPosition |
Returns or sets the true length text position |
UpperToleranceDegrees |
Returns or sets the upper angular tolerance in degrees |
UpperToleranceEnglish |
Returns or sets the upper english tolerance |
UpperToleranceMetric |
Returns or sets the upper metric tolerance |