TextOrientation Enumeration¶
-
class
NXOpen.Annotations.
TextOrientation
¶ Bases:
object
Specifies the dimension text orientation Enum Members
- the dimension line “
- “ByAngle”, ” Specifies dimension text at angle ” “Perpendicular”, ” Specifies dimension text perpendicular to the dimension line ” “SplitByDimensionLine”, ” Specifies dimenson text split by the dimension line ” “Last”, ” Last enum value. Should not be used. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.