ChamferForm Enumeration

class NXOpen.Annotations.ChamferForm

Bases: object

Specifies the chamfer dimension form Enum Members

Enum Member Enum Member Description
Symbol
C5
Size
5 x 5
SizeAngle
5 x 45
AngleSize
45 x 5
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.