ZeroToleranceDisplayStyle Enumeration¶
-
class
NXOpen.Annotations.
ZeroToleranceDisplayStyle
¶ Bases:
object
Specifies the 0 tolerance display style Enum Members
Enum Member Enum Member Description BasedOnUnits Zero tolerance display is tied to display unitsAsZero Always display zero tolerance as 0OmittedAndInlined Omit the display of zero tolerance and inline the remaining toleranceOmitted Omit the display of zero tolerance and maintain position of remaining tolerance-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-