FitAssemblyDisplayStyle Enumeration¶
-
class
NXOpen.Annotations.
FitAssemblyDisplayStyle
¶ Bases:
object
Specifies the limit and fit assembly display style This enum type is obsolete.
Deprecated since version NX11.0.0: Use
NXOpen.Annotations.FitAssemblyNewDisplayStyle
instead.Enum Members
Enum Member Enum Member Description SingleLine Display single lineTwoLinesCentered Display hole and shaft with dimension text centeredTwoLinesAligned Display hole and shaft with dimension text aligned-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-