Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static SplinePathBuilder.SplinePathSlackType |
SplinePathBuilder.SplinePathSlackType.ADDITIONAL_LENGTH
A interpolating (By-Poles) spline.
|
static SplinePathBuilder.SplinePathSlackType |
SplinePathBuilder.SplinePathSlackType.PERCENT_LENGTH
A control point (Thru-Point) spline.
|
SplinePathBuilder.SplinePathSlackType |
SplinePathBuilder.IsSplineSlackedData.slacktype |
static SplinePathBuilder.SplinePathSlackType |
SplinePathBuilder.SplinePathSlackType.UNDEFINED
The spline is undefined.
|
Modifier and Type | Method and Description |
---|---|
static SplinePathBuilder.SplinePathSlackType |
SplinePathBuilder.SplinePathSlackType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SplinePathBuilder.SplinePathSlackType |
SplinePathBuilder.SplinePathSlackType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SplinePathBuilder.SplinePathSlackType[] |
SplinePathBuilder.SplinePathSlackType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SplinePathBuilder.addSlackToSpline(SplinePathBuilder.SplinePathSlackType slackType,
Expression slackValue,
nxopen.Direction downDir)
License requirements: routing_base ("Routing Basic") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.