public static class SplinePathBuilder.SplinePathSlackType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADDITIONAL_LENGTH
A interpolating (By-Poles) spline.
|
static int |
_PERCENT_LENGTH
A control point (Thru-Point) spline.
|
static int |
_UNDEFINED
The spline is undefined.
|
static SplinePathBuilder.SplinePathSlackType |
ADDITIONAL_LENGTH
A interpolating (By-Poles) spline.
|
static SplinePathBuilder.SplinePathSlackType |
PERCENT_LENGTH
A control point (Thru-Point) spline.
|
static SplinePathBuilder.SplinePathSlackType |
UNDEFINED
The spline is undefined.
|
Modifier and Type | Method and Description |
---|---|
static SplinePathBuilder.SplinePathSlackType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SplinePathBuilder.SplinePathSlackType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SplinePathBuilder.SplinePathSlackType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SplinePathBuilder.SplinePathSlackType PERCENT_LENGTH
public static final SplinePathBuilder.SplinePathSlackType ADDITIONAL_LENGTH
public static final SplinePathBuilder.SplinePathSlackType UNDEFINED
public static final int _PERCENT_LENGTH
public static final int _ADDITIONAL_LENGTH
public static final int _UNDEFINED
public static SplinePathBuilder.SplinePathSlackType valueOf(int value)
public static SplinePathBuilder.SplinePathSlackType valueOf(String name)
public static SplinePathBuilder.SplinePathSlackType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.