public static class DesignRuleViolationViewer.OverrideOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NO
this shows that current violation is not overridden.
|
static int |
_YES
this shows that current violation is overridden violations
|
static DesignRuleViolationViewer.OverrideOption |
NO
this shows that current violation is not overridden.
|
static DesignRuleViolationViewer.OverrideOption |
YES
this shows that current violation is overridden violations
|
Modifier and Type | Method and Description |
---|---|
static DesignRuleViolationViewer.OverrideOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DesignRuleViolationViewer.OverrideOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DesignRuleViolationViewer.OverrideOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final DesignRuleViolationViewer.OverrideOption YES
public static final DesignRuleViolationViewer.OverrideOption NO
public static final int _YES
public static final int _NO
public static DesignRuleViolationViewer.OverrideOption valueOf(int value)
public static DesignRuleViolationViewer.OverrideOption valueOf(String name)
public static DesignRuleViolationViewer.OverrideOption[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.