Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static DesignRuleViolationViewer.OverrideOption |
DesignRuleViolationViewer.OverrideOption.NO
this shows that current violation is not overridden.
|
static DesignRuleViolationViewer.OverrideOption |
DesignRuleViolationViewer.OverrideOption.YES
this shows that current violation is overridden violations
|
Modifier and Type | Method and Description |
---|---|
DesignRuleViolationViewer.OverrideOption |
DesignRuleViolationViewer.overrideOptionValue()
Returns the value for design Rule Violation override option
if Yes: violation is overridden
if No: violation is not overridden
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
static DesignRuleViolationViewer.OverrideOption |
DesignRuleViolationViewer.OverrideOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DesignRuleViolationViewer.OverrideOption |
DesignRuleViolationViewer.OverrideOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DesignRuleViolationViewer.OverrideOption[] |
DesignRuleViolationViewer.OverrideOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DesignRuleViolationViewer.setOverrideOptionValue(DesignRuleViolationViewer.OverrideOption overrideOptionValue)
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.