public static class SimpleInterference.Result extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CAN_NOT_PERFORM_CHECK
An unknown
error has occured while performing
the interference check.
|
static int |
_INTERFERENCE_EXISTS
Interference
exists between the input bodies.
|
static int |
_NO_INTERFERENCE
No interference
exists between the input bodies.
|
static int |
_ONLY_EDGES_OR_FACES_INTERFERE
Only faces or edges interfere and no
solid interference exists between
the input bodies.
|
static SimpleInterference.Result |
CAN_NOT_PERFORM_CHECK
An unknown
error has occured while performing
the interference check.
|
static SimpleInterference.Result |
INTERFERENCE_EXISTS
Interference
exists between the input bodies.
|
static SimpleInterference.Result |
NO_INTERFERENCE
No interference
exists between the input bodies.
|
static SimpleInterference.Result |
ONLY_EDGES_OR_FACES_INTERFERE
Only faces or edges interfere and no
solid interference exists between
the input bodies.
|
Modifier and Type | Method and Description |
---|---|
static SimpleInterference.Result |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimpleInterference.Result |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimpleInterference.Result[] |
values()
Returns an array that contains the values for this enum.
|
public static final SimpleInterference.Result NO_INTERFERENCE
public static final SimpleInterference.Result ONLY_EDGES_OR_FACES_INTERFERE
public static final SimpleInterference.Result INTERFERENCE_EXISTS
SimpleInterference.getInterferenceResults()
to
obtain the pairs of faces interfering
or interference solid(s) created
between the input bodies.public static final SimpleInterference.Result CAN_NOT_PERFORM_CHECK
public static final int _NO_INTERFERENCE
public static final int _ONLY_EDGES_OR_FACES_INTERFERE
public static final int _INTERFERENCE_EXISTS
SimpleInterference.getInterferenceResults()
to
obtain the pairs of faces interfering
or interference solid(s) created
between the input bodies.public static final int _CAN_NOT_PERFORM_CHECK
public static SimpleInterference.Result valueOf(int value)
public static SimpleInterference.Result valueOf(String name)
public static SimpleInterference.Result[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.