Package | Description |
---|---|
nxopen.geometricanalysis |
Provides classes and interfaces for Geometric Analysis.
|
Modifier and Type | Field and Description |
---|---|
static SimpleInterference.Result |
SimpleInterference.Result.CAN_NOT_PERFORM_CHECK
An unknown
error has occured while performing
the interference check.
|
static SimpleInterference.Result |
SimpleInterference.Result.INTERFERENCE_EXISTS
Interference
exists between the input bodies.
|
static SimpleInterference.Result |
SimpleInterference.Result.NO_INTERFERENCE
No interference
exists between the input bodies.
|
static SimpleInterference.Result |
SimpleInterference.Result.ONLY_EDGES_OR_FACES_INTERFERE
Only faces or edges interfere and no
solid interference exists between
the input bodies.
|
Modifier and Type | Method and Description |
---|---|
SimpleInterference.Result |
SimpleInterference.performCheck()
Perform Interference Check.
|
static SimpleInterference.Result |
SimpleInterference.Result.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimpleInterference.Result |
SimpleInterference.Result.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimpleInterference.Result[] |
SimpleInterference.Result.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.