See: Description
Interface | Description |
---|---|
AnalysisManager |
Represents the collection of analysis commands
To obtain an instance of this class, refer to BasePart Created in NX5.0.0 |
AnalysisObject |
Represents an Analysis Object
This is an abstract class, and cannot be instantiated . |
AnalysisObjectCollection |
Create a AnalysisObjectCollection
To obtain an instance of this class, refer to AnalysisManager Created in NX5.0.0 |
CurveAnalysisCombsBuilder | Deprecated
Deprecated in NX8.5.0.
|
CurveAnalysisDisplay |
Represents a tool to control whether to show a curve's poles,knots,combs,peaks and inflections
To obtain an instance of this class, refer to AnalysisObjectCollection Created in NX6.0.0 |
CurveAnalysisInflectionsBuilder | Deprecated
Deprecated in NX8.5.0.
|
CurveAnalysisPeaksBuilder | Deprecated
Deprecated in NX8.5.0.
|
CurveAnalysisRecord | Deprecated
Deprecated in NX8.5.0.
|
CurveContinuity |
Represents a Curve Continuity Analysis builder
To create or edit an instance of this class, use CurveContinuityBuilder Created in NX7.0.0 |
CurveContinuityBuilder |
Represents a curve continuity builder
To create a new instance of this class, use AnalysisObjectCollection.createCurveContinuityBuilder(nxopen.DisplayableObject) Default values. |
CurveCurvatureAnalysis |
Represents a CurveCurvatureAnalysis builder
To create or edit an instance of this class, use CurveCurvatureAnalysisBuilder Created in NX7.0.0 |
CurveCurvatureAnalysisBuilder |
Represents a
CurveCurvatureAnalysis builder To create a new instance of this class, use AnalysisObjectCollection.createCurveCurvatureAnalysisBuilder(nxopen.DisplayableObject) Default values. |
DeviationChecking |
Represents a
DeviationChecking
To create a new instance of this class, use AnalysisManager.createDeviationCheckingObject() Created in NX6.0.0 |
DeviationGauge |
Deviation Gauge analysis object class
To create or edit an instance of this class, use DeviationGaugeBuilder Created in NX6.0.0 |
DeviationGaugeBuilder |
DeviationGaugeBuilder class
To create a new instance of this class, use AnalysisObjectCollection.createDeviationGaugeBuilder(nxopen.DisplayableObject) Default values. |
DraftAnalysis |
Represents a Draft Analysis builder
To create or edit an instance of this class, use DraftAnalysisBuilder Created in NX8.0.0 |
DraftAnalysisBuilder |
Represents a Draft Analysis builder
To create a new instance of this class, use AnalysisObjectCollection.createDraftAnalysisBuilder(nxopen.DisplayableObject) Default values. |
DupinBuilder |
The Dupin Indicatrix is a tool to geometrically display the surface curvature at a specified point on a surface.
|
ExamineGeometry |
Represents the Examine Geometry class
To create a new instance of this class, use AnalysisManager.createExamineGeometryObject() Created in NX5.0.0 |
FaceCurvatureAnalysis |
Represents a Face Curvature Analysis builder
To create or edit an instance of this class, use FaceCurvatureAnalysisBuilder Created in NX8.0.0 |
FaceCurvatureAnalysisBuilder |
Represents a
FaceCurvatureAnalysisBuilder builder. |
GapFlushness |
Gap and Flushness analysis object class
To create or edit an instance of this class, use GapFlushnessBuilder Created in NX5.0.0 |
GapFlushnessBuilder |
GapFlushnessBuilder class
To create a new instance of this class, use AnalysisObjectCollection.createGapFlushnessBuilder(nxopen.geometricanalysis.GapFlushness) Default values. |
GeometricProperties |
Represents the Geometric Properties class.
|
HighlightLinesAnalysis |
Represents a Highlight Lines Analysis object.
|
HighlightLinesAnalysisBuilder |
Represents a
HighlightLinesAnalysis
builder. |
LocalRadiusAnalysis |
Builder for Local Radius Analysis (formerly Dynamic Radius)
To create or edit an instance of this class, use LocalRadiusAnalysisBuilder Created in NX8.5.0 |
LocalRadiusAnalysisBuilder |
Represents a
LocalRadiusAnalysis builder To create a new instance of this class, use AnalysisObjectCollection.createLocalRadiusAnalysisBuilder(nxopen.geometricanalysis.LocalRadiusAnalysis) Default values. |
SectionAnalysisObject |
Represents a Section Analysis object.
|
SimpleInterference |
Represents the Simple Interference object.
|
SolidDensity |
Represents a
SolidDensity
To create a new instance of this class, use AnalysisManager.createSolidDensityObject() Created in NX5.0.0 |
SurfaceAnalysisDisplay |
Represents a tool control whether to show a surface's poles and knots
To obtain an instance of this class, refer to AnalysisObjectCollection Created in NX6.0.0 |
SurfaceContinuityAnalysis |
Represents a SurfaceContinuityAnalysis builder
To create or edit an instance of this class, use SurfaceContinuityAnalysisBuilder Created in NX6.0.0 |
SurfaceContinuityAnalysisBuilder |
Represents a
SurfaceContinuityAnalysis builder To create a new instance of this class, use AnalysisObjectCollection.createSurfaceContinuityAnalysisBuilder(nxopen.DisplayableObject) Default values. |
SurfaceIntersection |
Represents a SurfaceIntersection builder
To create or edit an instance of this class, use SurfaceIntersectionBuilder Created in NX7.5.0 |
SurfaceIntersectionBuilder |
Represents a
SurfaceIntersection builder To create a new instance of this class, use AnalysisObjectCollection.createSurfaceIntersectionBuilder(nxopen.DisplayableObject) Default values. |
Class | Description |
---|---|
CurveAnalysisCombsBuilder.DirectionOptionType |
Direction option types
|
CurveAnalysisDisplay.ShowFlagType | Deprecated
Deprecated in NX8.5.0.
|
CurveAnalysisInflectionsBuilder.DirectionOptionType |
Direction option types
|
CurveAnalysisPeaksBuilder.DirectionOptionType |
Direction option types
|
CurveAnalysisRecord.DirectionOptionType |
Direction option types
|
CurveCurvatureAnalysisBuilder.CalculationMethod |
Enumeration for needle calculation method
|
CurveCurvatureAnalysisBuilder.DisplayStyle |
Enumeration for needle display type
|
CurveCurvatureAnalysisBuilder.LabelValues |
Enumeration for label computation method
|
CurveCurvatureAnalysisBuilder.NeedleDirection |
Enumeration for needle direction type
|
CurveCurvatureAnalysisBuilder.ProjectionTypes |
Projection plane types
|
CurveCurvatureAnalysisBuilder.XyzTypes |
Enumeration for X, Y or Z projection plane
|
DeviationChecking.DeviationOptions |
the deviation type to be shown
|
DeviationChecking.Types |
the type of deviation checking to be performed
|
DeviationGaugeBuilder.AdditionalValuesLabelType |
This enum represents the Deviation Gauge Analysis Object additional values label type
|
DeviationGaugeBuilder.ColorPlotTypes |
This enum represents the Deviation Gauge Analysis Object color plot types
|
DeviationGaugeBuilder.MeasurementMethodType |
This enum represents the Deviation Gauge Analysis Object evaluation types
|
DeviationGaugeBuilder.MinMaxType |
This enum represents the Deviation Gauge Analysis Object min max type
|
DeviationGaugeBuilder.ReportingPerTypes |
This enum represents the Deviation Gauge Analysis Object reporting per setting
|
DeviationGaugeBuilder.XyzDirectionType |
This enum represents the Deviation Gauge Analysis Object X, Y, Z direction options
|
DraftAnalysisBuilder.DrawDirection |
define draw direction items
|
DraftAnalysisBuilder.SelectOutput |
define output options
|
ExamineGeometry.Check |
Types of checks
|
FaceCurvatureAnalysisBuilder.CurvatureTypes |
Represents the face curvature types.
|
FaceCurvatureAnalysisBuilder.DirectionTypes |
Methods of specifiying the direction for normal and section curvatures.
|
FaceCurvatureAnalysisBuilder.DisplayTypes |
Represents the display types.
|
FaceCurvatureAnalysisBuilder.ScaleTypes |
Represents the scaling types for curvature values.
|
GapFlushnessBuilder.DisplayOptions |
This enum represents Label Display Option type
|
GapFlushnessBuilder.EvaluationModes |
This enum represents evaluation mode
|
GapFlushnessBuilder.EvaluationTypes |
This enum represents the Gap and Flushness Analysis Object evaluation types
|
GapFlushnessBuilder.PanelTypes |
This enum represents panel type
|
GapFlushnessBuilder.SectionAlignments |
This enum represents cross-section alignment type
|
GapFlushnessBuilder.SectionCurveOptions |
This enum represents Cross Section Curves Options
|
GeometricProperties.CaeCurve |
CAE Edge/Curve Geometric Properties
|
GeometricProperties.CaeCurvePropertiesData |
This class holds the data returned from
GeometricProperties.getCaeCurveProperties(nxopen.NXObject, nxopen.Point3d) |
GeometricProperties.CaeFace |
CAE Face Geometric Properties
|
GeometricProperties.CaeFacePropertiesData |
This class holds the data returned from
GeometricProperties.getCaeFaceProperties(nxopen.NXObject, nxopen.Point3d) |
GeometricProperties.Edge |
Edge/Curve Geometric Properties
|
GeometricProperties.EdgePropertiesData |
This class holds the data returned from
GeometricProperties.getEdgeProperties(nxopen.NXObject, nxopen.Point3d) |
GeometricProperties.Entity |
Type of input entity for geometric properties.
|
GeometricProperties.Face |
Face Geometric Properties
|
GeometricProperties.FacePropertiesData |
This class holds the data returned from
GeometricProperties.getFaceProperties(nxopen.NXObject, nxopen.Point3d) |
GeometricProperties.OutputType |
Represents how to output geometric properties.
|
GeometricProperties.Status |
Status of computing geometric properties.
|
HighlightLinesAnalysisBuilder.DisplayMethods | Deprecated
Deprecated in NX8.0.0.
|
HighlightLinesAnalysisBuilder.LightPlacements |
light placement
|
HighlightLinesAnalysisBuilder.LightPlaneOptions |
light plane options
|
HighlightLinesAnalysisBuilder.Resolutions |
resolution options
|
HighlightLinesAnalysisBuilder.Types | Deprecated
Deprecated in NX8.0.0.
|
HighlightLinesAnalysisBuilder.Types2 |
four types of display methods
|
SimpleInterference.FaceInterferenceMethod |
Specifies to "find only first pair of interfering faces" or "all
pairs of interfering faces" between the input boides.
|
SimpleInterference.InterferenceMethod |
Specifies interference method, i.e., to highlight interfering
faces or create interference solid
|
SimpleInterference.Result |
Specifies the result of a simple interference check
|
SolidDensity.UnitsType |
Types of units for solid density
|
SurfaceAnalysisDisplay.ShowFlagType |
Show flag types
|
SurfaceContinuityAnalysisBuilder.CurvatureType |
Curvature types
|
SurfaceContinuityAnalysisBuilder.Types |
Two possible types for the dialog
|
SurfaceIntersectionBuilder.CalculationTypes |
Enumeration for needle calculation method
|
SurfaceIntersectionBuilder.DirectionTypes |
Enumeration for needle direction type
|
SurfaceIntersectionBuilder.LabelValues |
Enumeration for label computation method
|
SurfaceIntersectionBuilder.NormalTypes |
Enumeration for face normal
|
SurfaceIntersectionBuilder.ProjectionTypes |
Projection types
|
SurfaceIntersectionBuilder.ScalingTypes |
Enumeration for needle display type
|
SurfaceIntersectionBuilder.XyzTypes |
Enumeration for X, Y or Z projection plane
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.