public static class GeometricProperties.Status extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FAILED
Failed to find all geometric
properties
|
static int |
_INVALID_INPUT
Input specified is not
valid.
|
static int |
_SUCCESS
Success
|
static GeometricProperties.Status |
FAILED
Failed to find all geometric
properties
|
static GeometricProperties.Status |
INVALID_INPUT
Input specified is not
valid.
|
static GeometricProperties.Status |
SUCCESS
Success
|
Modifier and Type | Method and Description |
---|---|
static GeometricProperties.Status |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeometricProperties.Status |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeometricProperties.Status[] |
values()
Returns an array that contains the values for this enum.
|
public static final GeometricProperties.Status SUCCESS
public static final GeometricProperties.Status INVALID_INPUT
public static final GeometricProperties.Status FAILED
public static final int _SUCCESS
public static final int _INVALID_INPUT
public static final int _FAILED
public static GeometricProperties.Status valueOf(int value)
public static GeometricProperties.Status valueOf(String name)
public static GeometricProperties.Status[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.