Package | Description |
---|---|
nxopen.geometricanalysis |
Provides classes and interfaces for Geometric Analysis.
|
Modifier and Type | Field and Description |
---|---|
static GeometricProperties.Status |
GeometricProperties.Status.FAILED
Failed to find all geometric
properties
|
static GeometricProperties.Status |
GeometricProperties.Status.INVALID_INPUT
Input specified is not
valid.
|
GeometricProperties.Status |
GeometricProperties.FacePropertiesData.status
Return status
|
GeometricProperties.Status |
GeometricProperties.EdgePropertiesData.status
Return status
|
GeometricProperties.Status |
GeometricProperties.CaeFacePropertiesData.status
Return status
|
GeometricProperties.Status |
GeometricProperties.CaeCurvePropertiesData.status
Return status
|
static GeometricProperties.Status |
GeometricProperties.Status.SUCCESS
Success
|
Modifier and Type | Method and Description |
---|---|
GeometricProperties.Status |
GeometricProperties.listProperties(NXObject entityTag,
Point3d absPoint)
Displays the local properties of the specified object at the
given point in the listing window
License requirements: None. |
GeometricProperties.Status |
GeometricProperties.listProperties(Point3d absPoint)
Displays the local properties of
GeometricProperties.objectsForAnalysis() at the given point in
the listing window. |
static GeometricProperties.Status |
GeometricProperties.Status.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeometricProperties.Status |
GeometricProperties.Status.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeometricProperties.Status[] |
GeometricProperties.Status.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.