Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static EndCutBuilder.DraftTypes |
EndCutBuilder.DraftTypes.EXTEND
If this Draft Type is set, the EndCut face will split and the right side face will be tapered.
|
static EndCutBuilder.DraftTypes |
EndCutBuilder.DraftTypes.TRIM
If this Draft Type is set, the EndCut face will split and the left side face will be tapered.
|
Modifier and Type | Method and Description |
---|---|
EndCutBuilder.DraftTypes |
EndCutBuilder.draftType()
Returns the draft type.
|
static EndCutBuilder.DraftTypes |
EndCutBuilder.DraftTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EndCutBuilder.DraftTypes |
EndCutBuilder.DraftTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EndCutBuilder.DraftTypes[] |
EndCutBuilder.DraftTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EndCutBuilder.setDraftType(EndCutBuilder.DraftTypes draftType)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.