Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static EndCutBuilder.ConnectionTypes |
EndCutBuilder.ConnectionTypes.CONNECTED
If this Connection Type is set, the offset parameter will be ignored.
|
static EndCutBuilder.ConnectionTypes |
EndCutBuilder.ConnectionTypes.FLANGE_FREE
If this Connection Type is set, the offset parameter will be ignored.
|
static EndCutBuilder.ConnectionTypes |
EndCutBuilder.ConnectionTypes.SNIPED
If this Connection Type is set, the offset parameter can be used.
|
Modifier and Type | Method and Description |
---|---|
EndCutBuilder.ConnectionTypes |
EndCutBuilder.connectionType()
Returns the connection type.
|
static EndCutBuilder.ConnectionTypes |
EndCutBuilder.ConnectionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EndCutBuilder.ConnectionTypes |
EndCutBuilder.ConnectionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EndCutBuilder.ConnectionTypes[] |
EndCutBuilder.ConnectionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EndCutBuilder.setConnectionType(EndCutBuilder.ConnectionTypes connectionType)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.