Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static MiterOptions.TypeOptions |
MiterOptions.TypeOptions.NORMAL_TO_SOURCE_FACE
mitering is done along the normal to source face
|
static MiterOptions.TypeOptions |
MiterOptions.TypeOptions.NORMAL_TO_THICKNESS_FACE
mitering is done along the normal to thickness face
|
Modifier and Type | Method and Description |
---|---|
MiterOptions.TypeOptions |
MiterOptions.endType()
Returns the miter end type.
|
MiterOptions.TypeOptions |
MiterOptions.startType()
Returns the miter start type.
|
static MiterOptions.TypeOptions |
MiterOptions.TypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MiterOptions.TypeOptions |
MiterOptions.TypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MiterOptions.TypeOptions[] |
MiterOptions.TypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MiterOptions.setEndType(MiterOptions.TypeOptions endType)
Sets the miter end type.
|
void |
MiterOptions.setStartType(MiterOptions.TypeOptions startType)
Sets the miter start type.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.