public static class MiterOptions.TypeOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NORMAL_TO_SOURCE_FACE
mitering is done along the normal to source face
|
static int |
_NORMAL_TO_THICKNESS_FACE
mitering is done along the normal to thickness face
|
static MiterOptions.TypeOptions |
NORMAL_TO_SOURCE_FACE
mitering is done along the normal to source face
|
static MiterOptions.TypeOptions |
NORMAL_TO_THICKNESS_FACE
mitering is done along the normal to thickness face
|
Modifier and Type | Method and Description |
---|---|
static MiterOptions.TypeOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MiterOptions.TypeOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MiterOptions.TypeOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final MiterOptions.TypeOptions NORMAL_TO_SOURCE_FACE
public static final MiterOptions.TypeOptions NORMAL_TO_THICKNESS_FACE
public static final int _NORMAL_TO_SOURCE_FACE
public static final int _NORMAL_TO_THICKNESS_FACE
public static MiterOptions.TypeOptions valueOf(int value)
public static MiterOptions.TypeOptions valueOf(String name)
public static MiterOptions.TypeOptions[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.