Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static GussetBuilder.PlacementTypes |
GussetBuilder.PlacementTypes.FILL
Users will specify the spacing of Gussets on the selected bend face and software will calculate the number of occurances.
|
static GussetBuilder.PlacementTypes |
GussetBuilder.PlacementTypes.FIT
Users will specify the number of occurances of Gusset on the selected bend face and software will calculate the spacing.
|
static GussetBuilder.PlacementTypes |
GussetBuilder.PlacementTypes.FIXED
Users will specify the number of occurances and the spacing for Gussets on the selected bend face.
|
static GussetBuilder.PlacementTypes |
GussetBuilder.PlacementTypes.SINGLE
One Gusset will be created at an offset from an edge on the selected bend face.
|
Modifier and Type | Method and Description |
---|---|
GussetBuilder.PlacementTypes |
GussetBuilder.placementType()
Returns the placement type
Only use this option to edit gussets created prior to NX10. |
static GussetBuilder.PlacementTypes |
GussetBuilder.PlacementTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GussetBuilder.PlacementTypes |
GussetBuilder.PlacementTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GussetBuilder.PlacementTypes[] |
GussetBuilder.PlacementTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GussetBuilder.setPlacementType(GussetBuilder.PlacementTypes placementType)
License requirements: nx_sheet_metal ("NX Sheet Metal") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.