public static class GussetBuilder.PlacementTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FILL
Users will specify the spacing of Gussets on the selected bend face and software will calculate the number of occurances.
|
static int |
_FIT
Users will specify the number of occurances of Gusset on the selected bend face and software will calculate the spacing.
|
static int |
_FIXED
Users will specify the number of occurances and the spacing for Gussets on the selected bend face.
|
static int |
_SINGLE
One Gusset will be created at an offset from an edge on the selected bend face.
|
static GussetBuilder.PlacementTypes |
FILL
Users will specify the spacing of Gussets on the selected bend face and software will calculate the number of occurances.
|
static GussetBuilder.PlacementTypes |
FIT
Users will specify the number of occurances of Gusset on the selected bend face and software will calculate the spacing.
|
static GussetBuilder.PlacementTypes |
FIXED
Users will specify the number of occurances and the spacing for Gussets on the selected bend face.
|
static GussetBuilder.PlacementTypes |
SINGLE
One Gusset will be created at an offset from an edge on the selected bend face.
|
Modifier and Type | Method and Description |
---|---|
static GussetBuilder.PlacementTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GussetBuilder.PlacementTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GussetBuilder.PlacementTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final GussetBuilder.PlacementTypes SINGLE
public static final GussetBuilder.PlacementTypes FIT
public static final GussetBuilder.PlacementTypes FILL
public static final GussetBuilder.PlacementTypes FIXED
public static final int _SINGLE
public static final int _FIT
public static final int _FILL
public static final int _FIXED
public static GussetBuilder.PlacementTypes valueOf(int value)
public static GussetBuilder.PlacementTypes valueOf(String name)
public static GussetBuilder.PlacementTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.